|
London
central heating installer has halfed the time taken to install
controls since switching to Honeywell Smartfit.
“My
customers prefer the Smartfit controller which combines the
programmer and room thermostat in one unit”
BRACKNELL, UK,
3 April 2002 - Home heating
installer Robert Whiting of South London has halved the time to
install central heating controls since choosing Honeywell’s
Smartfit system over traditional controls. “It’s
fast and easy for me to install – and my customers love it,”
observed Robert, proprietor of RH Heating (84 Dumbarton Road,
London SW2 5LU). “They
particularly like the Smartfit controller which combines the
programmer and room thermostat in one unit,” he revealed.
Robert
always provides the best for his customers, so installs Smartfit
on all new central heating installations and upgrades where
possible. “It makes
upgrades particularly easy. Even when replacing a three-way valve,
I may recommend replacing the control system with Smartfit because
then householders have much better control of their central
heating and hot water, as well as the convenience of a single
control unit. It
doesn’t take long to install a Smartfit system due to its
snap-on valve actuator and plug-in electrical connections – and
I leave behind a very happy customer.”
Smartfit
installer packs contain everything needed for an installation
including valves, a cylinder sensor, a
controller and a base unit with plug-in connections and
ready-wired cables ready to plug in.
Some
80 per cent of RH Heating’s installations are directly for
householders and the remainder is contract work, notably for
London borough councils.
RH
Heating is one of many installers, housing associations and
councils throughout the UK that have changed to Smartfit, whose
circuits uniquely use 12 volts or less, not mains voltage, and are
centred on a connection box that provides plug-in or simple 2-wire
connection for all space heating and hot water controls.
Installers simply connect the two-wire room unit, plug in
the valves and cylinder sensor, and the system is complete.
Valve actuators simply snap on and are common to all valves
in the range. There
is no need for a wiring diagram and it is virtually impossible to
install a Smartfit system incorrectly.
Contacts for reader enquiries:
Pauline
Wetherell,
Honeywell Control Systems Ltd.,
Honeywell House, Arlington Business Park,
Bracknell, Berkshire RG12 1EB.
Telephone: 01344 656000.
Fax: 01344 656240. Email: uk.infocentre@honeywell.com
Web: www.honeywell.com/uk/homes.htm
Robert
Whiting, RH Heating, 84 Dumbarton Road, London SW2 5LU. Telephone:
020 8678 6217.
Honeywell is a US$24-billion diversified
technology and manufacturing leader, serving customers worldwide with aerospace products
and services; control technologies for buildings, homes and industry; automotive products;
power generation systems; specialty chemicals; fibres; plastics; and electronic and
advanced materials. The company is a leading provider of software and solutions, and
Internet e-hubs including MyPlant.com, MyFacilities.com and MyAircraft.com (joint venture
with United Technologies and i2 Technologies). Honeywell employs approximately 120,000
people in 95 countries and is traded on the New York Stock Exchange under the symbol HON,
as well as on the London, Chicago and Pacific stock exchanges. It is one of the 30 stocks
that make up the Dow Jones Industrial Average and is also a component of the Standard
& Poors 500 Index. Additional information on the company is available on the
Internet at www.honeywell.com.
This release contains forward-looking
statements as defined in Section 21E of the Securities Exchange Act of 1934, including
statements about future business operations, financial performance and market conditions.
Such forward-looking statements involve risks and uncertainties inherent in business
forecasts.
# # #
Honeywell Control Systems
Ltd
Honeywell House, Arlington Business Park
Bracknell, Berkshire RG12 1EB
01344 656000. Fax: 01344 656240.
Enquiries e-mail: uk.infocentre@honeywell.com
Web: www.honeywell.com/uk
|