Home>Worldwide Sites


SEARCH

SITE MAP

HONEYWELL IN THE NEWS

HONEYWELL IN THE UK

SOLUTIONS FOR:
- Homes

- Buildings

- Industry

- Aviation

-Sensing & Control

FORTHCOMING EVENTS

YEAR 2000


 

IN THE NEWS
 
Editorial contact: Royer Slater
Honeywell Control Systems Ltd
Direct to desk: 01344 656379
Ref: UK05/01

MicroniK 200 controller series is Honeywell's cost-effective solution to decentralised HVAC control for buildings

BRACKNELL, UK, 12 February 2001 - Honeywell's new MicroniK 200 controller series is a cost-effective solution to decentralised control in heating, ventilating and air conditioning applications in offices, public buildings and retail premises. Digital control technology and a user-friendly operating concept allow fast configuration and accurate setting of parameters.

Typical applications include temperature sequence or cascade control with heating, mixed air dampers and cooling; and temperature cascade control with heating, energy recovery system and cooling.

The Honeywell MicroniK 200 controller is available as either a temperature controller or universal input controller. There is a choice of three output types: one floating 2 or 3 stage on/off output; three floating 2, 3, 4, 6 or 15 stage on/off outputs; or analogue 0 to 10Vdc. Three temperature sensor inputs are provided (main, limit or cascade and outside temperature compensation) and three digital inputs (plant system on/off, occupancy and freeze protection).

The unit measures just 198 x 130 x 37mm (H x W x D) and features a liquid crystal display, a rotary potentiometer, and four push-buttons for program setting by means of an intuitive menu loop shown graphically on the front of the unit for reference.

Readers can request further details from: Honeywell Control Systems Ltd., Honeywell House, Arlington Business Park, Bracknell, Berkshire RG12 1EB. Tel: 01344 656000. Fax: 01344 656240. E-mail: uk.infocentre@honeywell.com
Web: www.honeywell.com/uk

Honeywell Home & Building Control is a US$5 billion business that provides products and services to create efficient, safe, comfortable environments. The business offers controls for heating, ventilation, humidification and air-conditioning equipment, security and fire alarm systems, home automation systems, energy-efficient lighting controls and building management systems and services.

Honeywell is a US$24-billion diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; power generation systems; specialty chemicals; fibres; plastics; and electronic and advanced materials. The company is a leading provider of software and solutions, and Internet e-hubs including MyPlant.com, MyFacilities.com and MyAircraft.com (joint venture with United Technologies and i2 Technologies). Honeywell employs approximately 120,000 people in 95 countries and is traded on the New York Stock Exchange under the symbol HON, as well as on the London, Chicago and Pacific stock exchanges. It is one of the 30 stocks that make up the Dow Jones Industrial Average and is also a component of the Standard & Poor’s 500 Index. Additional information on the company is available on the Internet at www.honeywell.com.

This release contains forward-looking statements as defined in Section 21E of the Securities Exchange Act of 1934, including statements about future business operations, financial performance and market conditions. Such forward-looking statements involve risks and uncertainties inherent in business forecasts.

# # #

Honeywell Control Systems Ltd
Honeywell House, Arlington Business Park
Bracknell, Berkshire RG12 1EB
01344 656000. Fax: 01344 656240.
Enquiries e-mail: uk.infocentre@honeywell.com
Web: www.honeywell.com/uk

Editorial contact: Royer Slater
Honeywell Control Systems Ltd
Direct to desk: 01344 656379
royer.slater@honeywell.com




Copyright © 1999 Honeywell. All rights reserved