Home>Worldwide Sites


SEARCH

SITE MAP

HONEYWELL IN THE NEWS

HONEYWELL IN THE UK

SOLUTIONS FOR:
- Homes

- Buildings

- Industry

- Aviation

-Sensing & Control

FORTHCOMING EVENTS

YEAR 2000



IN THE NEWS
 

Honeywell issues it's latest comprehensive catalogue of products for domestic heating and plumbing.

Published both online and as a spiral - bound book.

BRACKNELL, UK, 21 FEBRUARY 2002 - Honeywell has published its latest comprehensive catalogue of products for the domestic heating and plumbing market both online at www.honeywell.com/uk/homes.htm and as a spiral-bound book.

Issue 8 of the catalogue provides a wealth of information on Honeywell’s comprehensive range, from thermostats to water and gas valves, from time switches to boiler management systems.  Each product is described in terms of its features, application, installation and specification.

The latest catalogue includes full details of the Honeywell Smartfit system, which has been widely acknowledged by the domestic heating industry and its trade press as a revolutionary development in home heating and hot water control.  Smartfit is available as Y Plan and S Plan systems packs with all the components required for a complete installation.  The catalogue also provides details of options such as a frost protection kit, and remote sensor and set point modules.

Smartfit is faster and easier to install than a conventional home control system.  It features plug-in connections and all system wiring connections are low voltage and polarity-free. With Smartfit, there is no need for a wiring diagram: installers simply connect the two-wire room unit, plug in the valves and cylinder sensor and the control system is complete.

Readers can view Honeywell’s new catalogue online at www.honeywell.com/uk/homes.htm and can request a printed, spiral-bound copy from: Pauline Wetherell, Honeywell Control Systems Ltd, Honeywell House, Arlington Business Park, Bracknell, Berkshire RG12 1EB.  Tel: 01344 656000.  Fax: 01344 656240.  

Email: uk.infocentre@honeywell.com      

Web: www.honeywell.com/uk/homes.htm

Honeywell is a US$24-billion diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; power generation systems; specialty chemicals; fibres; plastics; and electronic and advanced materials. The company is a leading provider of software and solutions, and Internet e-hubs including MyPlant.com, MyFacilities.com and MyAircraft.com (joint venture with United Technologies and i2 Technologies). Honeywell employs approximately 120,000 people in 95 countries and is traded on the New York Stock Exchange under the symbol HON, as well as on the London, Chicago and Pacific stock exchanges. It is one of the 30 stocks that make up the Dow Jones Industrial Average and is also a component of the Standard & Poor’s 500 Index. Additional information on the company is available on the Internet at www.honeywell.com.

This release contains forward-looking statements as defined in Section 21E of the Securities Exchange Act of 1934, including statements about future business operations, financial performance and market conditions. Such forward-looking statements involve risks and uncertainties inherent in business forecasts.

# # #

Honeywell Control Systems Ltd
Honeywell House, Arlington Business Park
Bracknell, Berkshire RG12 1EB
01344 656000. Fax: 01344 656240.
Enquiries e-mail: uk.infocentre@honeywell.com
Web: www.honeywell.com/uk

Contacts: Matthew Gordon
Honeywell Control Systems Ltd
Tel : 01344 656000
matthew.gordon@honeywell.com
Royer Slater
Slater Communications
Tel : 01483 481364
response@slatercomms.co.uk

Ref: HC
008




Copyright © 1999 Honeywell. All rights reserved