|
Honeywell introduces Avaya's iPatchTM monitoring system;
helps manage voice and data cable networks
BIRMINGHAM, UK, 21 MAY 2001 – At IFSEC 2001, Honeywell provides the first
UK demonstration of Avaya's new iPatchTM
monitoring system, an intelligent system
that broadens cable network management monitoring capabilities. Honeywell is
Avaya's only European Prestige VAR (value added reseller).
The iPatch system gives real-time status of voice and data port connections,
and speeds and improves accuracy of patch cord installations.
Through a combination of software and electronically-enabled hardware, the
iPatch system increases productivity and precision in maintaining networks by
continuously monitoring and recording the status of port connections at the patch
panel. The iPatch system tracks the location, availability and use of ports and creates a
connectivity map showing patch cord links between the network equipment and user
voice and data workstation outlets. The connectivity map can be viewed at any time
from a remote PC or from the iPatch system equipment in the telecommunications
room. The iPatch system automatically updates the map every time a port change
occurs, helping to assure that system administrators always have an accurate picture
of their status. System administrators can use their computer to easily schedule work
orders, track their fulfillment and receive immediate alerts when unauthorised port
connections or disconnections occur.
"Most businesses today rely on paper records or electronic spread sheets to
keep track of changes to port connections," said George Brooks, iPatch system
product manager, Avaya. "Over time, the records can get out of sync with the reality.
The only way to confirm the actual status may be to go physically to the
telecommunications room and trace patch cord connections by hand – a time-
consuming task with uncertain consequences. Incorrect information can trigger costly
mistakes that disrupt business.
The iPatch system eliminates questionable records, making it easier to quickly
and accurately perform patch cord moves, adds and changes and thus minimising the
risk of unnecessary downtime."
The iPatch system guides technicians with visual and audio prompts as they
make patch cord connections. iPatch system panels are equipped with trace buttons
and LEDs above each port. The panels communicate with iPatch system Rack
Managers outfitted with LCD displays. When system administrators generate work
orders for moves, adds and changes, the Rack Managers display the involved ports on
the LCD, and the LEDs above both of the ports are lit. Technicians can also identify
and display both ends of installed patch cords using one-button tracing. An audible
"positive" or "negative" sound informs technicians if a connection is properly
completed.
The iPatch system accommodates a standard modular patch cord, and consists
of iPatch System Manager Software, iPatch Network Manager, iPatch Rack Managers
and iPatch Panels. The iPatch Panel is built on the SYSTIMAX1100 panel design and
is available in 24 or 48 port configurations for SYSTIMAX GigaSPEED? or
SYSTIMAX Power Sum applications. A typical configuration includes a single
Network Manager supporting up to 99 iPatch Rack Managers, which support up to 40
iPatch 24-port panels.
Avaya's SYSTIMAX Structured Connectivity Solutions, Avaya's premier
structured cabling system for commercial applications, is also available through
Honeywell, as Avaya's only European Prestige VAR (value added reseller).
SYSTIMAX is an open, modular cabling solution, capable of simultaneously carrying
data, voice, video and intelligent building management applications. The SYSTIMAX
family of products, including the SYSTIMAX GigaSPEED copper solution as well as
OptiSPEED™ and LazrSPEED? fibre solutions are backed by an industry-leading
product warranty and applications assurance guarantee.
Readers can request further details from Honeywell Home and Building
Control, Honeywell House, Arlington Business Park, Bracknell, Berkshire
RG12 1EB. Tel: 01344 656000. Fax: 01344 656240. E-mail:
uk.infocentre@honeywell.com Web: myserviceandsolutions.co.uk
Honeywell Home & Building Control is a US$5 billion business that provides
products and services to create efficient, safe, comfortable environments. The business offers
controls for heating, ventilation, humidification and air-conditioning equipment, security and
fire alarm systems, home automation systems, energy-efficient lighting controls and building
management systems and services.
Honeywell is a US$25-billion diversified technology and manufacturing leader,
serving customers worldwide with aerospace products and services; control technologies for
buildings, homes and industry; automotive products; power generation systems; specialty
chemicals; fibers; plastics; and electronic and advanced materials. The company is a leading
provider of software and solutions and Internet e-hubs including MyPlant.com and
MyFacilities.com, and it is a founding member of Cordiem, LLC, an aerospace industry
business-to-business Internet exchange and applications service provider. Honeywell
employs approximately 125,000 people in 95 countries and is traded on the New York Stock
Exchange under the symbol HON, as well as on the London, Chicago and Pacific stock
exchanges. It is one of the 30 stocks that make up the Dow Jones Industrial Average and is
also a component of the Standard & Poor's 500 Index. Additional information on the
company is available on the Internet at www.honeywell.com.
This release contains forward-looking statements as defined in Section 21E of the Securities Exchange
Act of 1934, including statements about future business operations, financial performance and market
conditions. Such forward-looking statements involve risks and uncertainties inherent in business
forecasts as further described in our filings under the Securities Exchange Act.
# # #
Honeywell
Home and business Control
Honeywell House, Arlington Business Park
Bracknell, Berkshire RG12 1EB
Tel: 01344 656000. Fax: 01344 656240.
Enquiries e-mail: uk.infocentre@honeywell.com
Web: www.honeywell.com/uk
www.myserviceandsolutions.co.uk
Contact: Royer Slater
Honeywell Control Systems Ltd
Direct to desk: 01344 655203royer.slater@honeywell.com Ref:
UK29/01
|