|
Honeywell plays a vital
role in conserving the Mary Rose and protecting its treasures in The
Mary Rose Museum
BRACKNELL,
UK, 16 JULY 2001 –
Sophisticated monitoring and control technology from
Honeywell, plus a 24-hour remote monitoring service donated by
Honeywell’s UK Response Centre, is helping to preserve a unique
and priceless piece of British heritage – the hull and artefacts
from Henry VIII’s flag-ship, the “Mary Rose”.
After the ship sank in 1545 near the entrance to Portsmouth
Harbour, layers of silt protected her contents and half of the
hull. Many artefacts
and 3,000 timbers were removed from the wreck site during the
eleven years before the empty hull itself was raised in 1982.
The
hull of the Mary Rose is now the subject of the single largest
archaeological conservation project in the world.
The Mary Rose Trust, a registered charity with H.R.H.
Prince Charles as President, is actively conserving the ancient
oak timbers within a dry dock in Portsmouth’s Historic Dockyard.
The hull is housed beneath a double-skinned, thermally
insulated protective roof. It
is sprayed continuously with an aqueous solution of Polyethylene
Glycol (PEG), which is penetrating deep into the delicate cell
walls of the timber. By
replacing water in the cells, the PEG will minimise distortion of
the hull when it is eventually dried out in about ten years time.
A
Honeywell Excel 5000 management system monitors and controls 250
parameters and interfaces with an Excel Building Supervisor
building management system. Its duties include monitoring spray pumps, filter pressure,
tank level and many other variables; as well as regulating the
heating system within the ship hall and the heating and
ventilation system to the glass-fronted visitors’ viewing
gallery.
A
second, much smaller Honeywell system is installed within the Mary
Rose exhibition building: this provides ambient heating and air
conditioning as well as precise temperature and humidity control
within numerous sealed glass-fronted display cabinets, in which
some 1000 relics and treasures from the ship are on public
display.
“The
hull treatment process must be continuous to prevent it drying
out, so we are grateful that Honeywell’s Response Centre in
Bracknell monitors the Mary Rose’s BMS around the clock,”
explained conservation scientist Dr Mark Jones, Head of
Collections with The Mary Rose Trust.
“We go home at night knowing we’re in good hands.
At the first sign of a problem, Honeywell’s Response
Centre will alert our engineers so we can take immediate action
– and Honeywell generously does not charge us for this wonderful
service.”
“The
Honeywell Excel 5000 building management system has been terrific
throughout – we have had no problems.
Honeywell upgraded it in 1999 because of the Millennium bug
and, as a result, we now benefit from a new graphical interface.
We get a first-class service from Honeywell’s service
engineers, who are always helpful and friendly.
Their contribution is just as important to us as Honeywell
allowing us to use the services of its Response Centre without
charge. We have
routine service visits for the museum and ship hall and, if
there’s a problem at any time, we can speak to Honeywell’s
engineers on the phone. In
many cases, we are able to fix a problem ourselves but, if not,
the response from Honeywell’s service engineers is fantastic.”
Revealed
the Trust’s Conservation Manager, Glenn McConnachie, “The main
Honeywell BMS is a huge system controlling the PEG spray system,
PEG heat exchangers, pumps, boilers and environments.
The critical alarms that extend to Honeywell’s 24-hour
Response Centre are associated with the hull conservation process
and would indicate a spray system failure.
Specifically, the critical alarms are low level in the sump
tank, into which the spray solution drains for re-circulation, and
high and low pressures within the spray system.
These pressure abnormalities would most likely be due to,
respectively, a system blockage or a blow-out in the spray
system.”
The
Mary Rose Trust also has a freeze drier unit, operating at minus
30 degrees Celsius and low pressure, that is used to preserve
small archaeological treasures.
This exacting conservation process is ensured through links
to the Honeywell Excel 5000 system, which extends further critical
alarms to the Honeywell Response Centre for 24-hour monitoring.
The
Mary Rose Trust (President: H.R.H The Prince of Wales, K.G., K.T.,
P.C., G.C.B) is a Registered Charity and Limited Liability Company
which was founded in 1979 to manage the tasks of surveying,
excavating, recovering and displaying the ship and her contents. It is an international museum of Tudor life, and a recognised
centre of excellence for maritime archaeology and the conservation
of material recovered from underwater.
Honeywell
Home & Building Control is a US$5 billion business that
provides products and services to create efficient, safe,
comfortable environments. The business offers controls for
heating, ventilation, humidification and air-conditioning
equipment, security and fire alarm systems, home automation
systems, energy-efficient lighting controls and building
management systems and services.
Honeywell
is a US$25-billion diversified technology and manufacturing
leader, serving customers worldwide with aerospace products and
services; control technologies for buildings, homes and industry;
automotive products; power generation systems; speciality
chemicals; fibres; plastics; and electronic and advanced
materials. Honeywell employs approximately 120,000 people in 95 countries
and is traded on the New York Stock Exchange under the symbol HON,
as well as on the London, Chicago and Pacific stock exchanges. It is one of the 30 stocks that make up the Dow Jones
Industrial Average and is also a component of the Standard &
Poor’s 500 Index. Additional
information on the company is available on the Internet at
www.honeywell.com.
This
release contains forward-looking statements as defined in Section
21E of the Securities Exchange Act of 1934, including statements
about future business operations, financial performance and market
conditions. Such
forward-looking statements involve risks and uncertainties
inherent in business forecasts as further described in our filings
under the Securities Exchange Act.
Honeywell Control Systems
Ltd
Honeywell House, Arlington Business Park
Bracknell, Berkshire RG12 1EB
01344 656000. Fax: 01344 656240.
Enquiries e-mail: uk.infocentre@honeywell.com
Web: www.honeywell.com/uk
Editorial contact: Royer Slater
Honeywell Control Systems Ltd
Direct to desk: 01344 656000
royer.slater@honeywell.com |