Home>Worldwide Sites


SEARCH

SITE MAP

HONEYWELL IN THE NEWS

HONEYWELL IN THE UK

SOLUTIONS FOR:
- Homes

- Buildings

- Industry

- Aviation

-Sensing & Control

FORTHCOMING EVENTS

YEAR 2000



IN THE NEWS
 

Automatic Time Set feature uses national radio signal to ensure Smartfit central heating control keeps accurate time.

Another Smartfit that adds to happy customers profitable installation and enhanced reputation.

BRACKNELL, UK, 19 SEPTEMBER 2002 An Automatic Time Set (ATS) option has been added to the controller at the heart of Honeywell’s Smartfit home central heating and hot water control system.  With the ATS option, the Smartfit Room Unit will have the most accurate clock in the house and the user or installer never need set its time again. 

The Smartfit ATS electronics recognise the national radio time signal transmitted from Rugby by the National Physical Laboratory (NPL) and sets the correct time and day.  Every day the signal is checked to ensure the Smartfit controller keeps to the precise time.  The Smartfit clock is adjusted automatically when the time changes between GMT and BST. 

Honeywell Smartfit has already revolutionised the heating control industry through its low voltage wiring and plug-in control connections that minimise the chance of errors and make wiring quicker and simpler.  The ATS option requires no extra wiring and the radio signal can be received throughout the British Isles. 

Smartfit’s simplicity of installation already increases installers’ productivity by removing the difficulty of wiring a home central heating system, reducing installation time and by providing diagnostic codes that the householder can read over the phone to simplify fault-finding in the event of failure.  With ATS, the installer will never get a call-back to reset the clock. 

All these features, coupled with the established Honeywell renown for quality and reliability, add up to happy customers, profitable installation and enhanced reputation.

Smartfit systems are supplied in Y-Plan and S-Plan options, whilst the stylish Smartfit controller is available in 24-hour and 7-day versions.

Full details of this and all Honeywell heating products may be found on the web at www.honeywell.com/uk/homes.htm; click on the Technical Catalogue or Application Guides for more information.

Written enquiries : Honeywell Control Systems Ltd, Honeywell House, Arlington Business Park, Bracknell, Berkshire RR12 1EB. Tel : 01344 656000. Fax : 01344 656240. Installers' Technical Helpline : 08457 678999.
E- Mail : uk.infocentre@honeywell.com
Web : www.honeywell.com/uk/homes.htm

Honeywell is a US$24-billion diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; power generation systems; speciality chemicals; fibres; plastics; and electronic and advanced materials.  Honeywell employs approximately 115,000 people in 95 countries and is traded on the New York Stock Exchange under the symbol HON, as well as on the London, Chicago and Pacific stock exchanges.  It is one of the 30 stocks that make up the Dow Jones Industrial Average and is also a component of the Standard & Poor’s 500 Index.  Additional information on the company is available on the Internet at www.honeywell.com.

This release contains forward-looking statements as defined in Section 21E of the Securities Exchange Act of 1934, including statements about future business operations, financial performance and market conditions.  Such forward-looking statements involve risks and uncertainties inherent in business forecasts as further described in our filings under the Securities Exchange Act

# # #

Honeywell Control Systems Ltd
Honeywell House, Arlington Business Park
Bracknell, Berkshire RG12 1EB
01344 656000. Fax: 01344 656240.
Enquiries e-mail: uk.infocentre@honeywell.com
Web: www.honeywell.com/uk

Contacts: Matthew Gordon
Honeywell Control Systems Ltd
Tel : 01344 656000

matthew.gordon@honeywell.com
Royer Slater
Slater Communications
Tel : 01483 481364
Fax : 01483 854391
response@slatercomms.co.uk

Ref: HC
045




Copyright © 1999 Honeywell. All rights reserved



 

Honeywell's 7  - day and 24 - hour Smartfit Room units now have an Automatic Time Set (ATS) option  means that Smartfit will have the most accurate clock in the house and the usre or the installer never need set the time again.