HC900 Product Support
Technical Tips
Firmware Downloads
Download any necessary Zip files to you hard drive and expand them using Winzip®, or equivalent, software. Included in all zip files is a Readme file with instructions on how to proceed
NOTE:Version 4.1 firmware can only be installed in CPU and Scanner modules designed with the NS9750 microprocessor
(produced after S/N 06xx). Modules with firmware 2.1 or older will not function and
cannot be upgraded with this firmware.
Please be aware, the CPU upgrade files previously provided in .zip formats
have been changed to the .msi format. Download the necessary files to your PC, then
double click on the file and it will self install to the C:/Program files/HC900 firmware folder.
Also, the V 4.1 Scanner and OI upgrades are now included in the HC Designer upgrade
and can be found in the C:/Program files/HC900 firmware folder.
|
File Name |
Description |
Date(MM/DD/YY) |
Filesize |
Comments |
|
C30V4_101.msi |
C30 CPU Firmware upgrade |
11/27/06 |
1.26 MB |
Small Capacity
CPU |
|
C50V4_101.msi |
C50 CPU Firmware
upgrade |
11/27/06 |
1.29 MB |
Medium Capacity
CPU |
|
C70V4_101.msi |
C70 CPU Firmware upgrade |
11/27/06 |
1.29 MB |
Large Capacity
CPU |
|
C70RV4_101.msi |
C70R CPU Firmware upgrade |
11/27/06 |
1.47 MB |
Redundant CPU |
|
HCDesigner4_101.zip |
HC Designer version 4.101 |
02/02/07 |
45.9 MB |
PC configuration SW |
|
HC DesignerDemo4_100.zip |
HC DesignerDemo version 4.100 |
11/27/06 |
10.3 MB |
PC configuration demo package |
|
HCUtilities4_101.zip |
HC Utilities version 4.101 |
02/02/07 |
78.8 MB |
PC utilities software |
NOTE:Version 4.0
firmware can only be installed in modules designed with the NS9750
microprocessor (produced after S/N 06xx). Modules with firmware 2.1 or
older will not function and cannot be upgraded with this
firmware.
|
File Name |
Description |
Date(MM/DD/YY) |
Filesize |
Comments |
|
C30V4_002.zip |
C30 CPU Firmware
upgrade |
09/01/06 |
1.18 MB |
Small Capacity
CPU |
|
C50V4_002.zip |
C50 CPU Firmware
upgrade |
09/01/06 |
1.21 MB |
Medium Capacity
CPU |
|
C70V4_003.zip |
C70 CPU Firmware
upgrade |
09/01/06 |
1.22 MB |
Large Capacity
CPU |
|
C53V4_0.zip |
C53 Scanner Firmware
upgrade |
07/28/06 |
1.19 MB |
Single port I/O
expansion module-(Non redundant) |
|
C70RV4_002.zip |
C70R CPU Firmware
upgrade |
09/01/06 |
1.40 MB |
Redundant CPU |
|
C73RV4_0.zip |
C73R Scanner Firmware
upgrade |
07/28/06 |
1.36 MB |
Redundant port I/O
expansion module |
|
OI_559v4_0.zip |
OI software for the 559 |
08/01/06 |
411 KB |
small OI |
|
OI_1042v4_0.zip |
OI software for the 1042 |
08/01/06 |
493 KB |
large OI |
These files allow users to UPGRADE to the latest version of release 2.1, HC900 modules. Please note, for systems
using a C50 CPU and Scanner modules, both the CPU modules and Scanners must be
updated to the latest versions to be compatible. Version 3.1, OI firmware is compatible
with Version 2.1, 2.3 and 2.4, C30/C50/C70 controllers and Version 1.0, C70R systems.
|
File Name |
Description |
Date (MM/DD/YY) |
Filesize |
Comments |
|
OI_559v3_1.zip |
OI software for the 559 |
01/03/06 |
401 KB |
small OI |
|
OI_1042v3_1.zip |
OI software for the 1042 |
01/03/06 |
481 KB |
large OI |
|
HC930v02_109.zip |
CPU 30 firmware Upgrade |
04/11/05 |
1.07 MB |
small capacity CPU |
|
HC900v02_109.zip |
CPU 50 firmware Upgrade |
04/11/05 |
1.34 MB |
large capacity CPU |
|
SC900v02_104.zip |
Scanner firmware Upgrade |
04/11/05 |
551 KB |
used in extension I/O racks |
HC900, C30 and C50 Processor and C53 Scanner modules produced prior to Jan. 2006
(SN 0601Y…)were based on a Net40 microprocessor. HC900, C30, C50 and C70 Processors and C53 Scanners produced after Jan. 2006 (SN 0601Y…)
are based on a NS9750 microprocessor.Firmware version 2.3 is the initial release of the modules based on the NS9750 microprocessor
and can only be downloaded to NS9750 based modules. The newer modules with version 2.3
firmware are compatible with Net40 based C30/C50 processors of Version 2.109 and C53
Scanners of Version 2.104 and can be used as direct replacements should one of the Net 40 based modules fail. As new HC900 firmware releases occur for the NS9750 based modules, users
needing to replace Net 40 based modules will need to downgrade the firmware in the new module,
to be compatible. The table below provides users with Version 2.3 for the respective modules.
Please note:when loading firmware to a NS9750 based Scanner module, please select the
appropriate file based on the Controller type through which the Scanner code will be
downloaded. Also, Scanner modules with a versions greater than V 2.3 will not initially appear in
the monitor mode; however, the V 2.3 firmware can still be downloaded.
|
File Name |
Description |
Date(MM/DD/YY) |
Filesize |
Comments |
|
HC930V2_3.zip |
CPU 30 firmware Upgrade |
03/10/06 |
1.59MB |
small capacity CPU |
|
HC950V2_3.zip |
CPU 50 firmware Upgrade |
03/10/06 |
1.63 MB |
medium capacity CPU |
|
HC970V2_3.zip |
CPU 70 firmware Upgrade |
03/10/06 |
1.64 MB |
large capacity CPU |
|
SC953Net40V2_3.zip |
Scanner firmware Upgrade for download via Net40 CPU |
03/10/06 |
780 KB |
used in extension I/O racks |
|
SC953NS9750V2_3.zip |
Scanner firmware Upgrade for download via NS9750 CPU |
03/10/06 |
895 KB |
used in extension I/O racks |
Application Notes
Field Notices
|
Number |
Description |
Date (MM/DD/YY) |
|
100 |
CPU firmware 1.02 |
7/12/02 |
|