UDC 2500 Product Software Download
Important: Before attempting to
download any firmware, it is necessary to obtain the current version of software in the UDC 2500
Step 1 of 4
Determining the software version
|
Procedure for Identifying the Software Version
|
|
Step
|
Operation
|
Press
|
Result
|
|
1
|
Select STATUS Set Up Group
|
|
Upper Display = READ
Lower Display = STATUS
|
|
2
|
Read the software version
|
|
You will see
Upper Display = 25xx
(xx is the Software Version)
Lower Display = VERSION
|
|
Step 2 of 4
Download "Code Download" program.
Note: Below are minimum requirements for operational environment of
Process Instrument Code Download:
| Operating System: |
Windows 2000 sp2
Windows XP sp
Windows NT sp6
Pocket PC 2002 or later |
| CPU: |
Intel x86 processor, Pocket PC with Intel
PXA250/PXA255 CPU. |
| Memory: |
64MB PC / 32 Meg PPC
(Required memory size will vary depending on usage) |
| Display: |
800 x 600, 64K (16 bit), High color or up |
| Click here to download Process Instrument Code Download
|
|
Download any necessary Zip files to your hard drive and expand them
using WinZip® or equivalent software.
Included in all zip files is a PDF file with instructions on how to proceed. |
Step 3 of 4
Download the appropriate binary file to the local hard drive on the PC.
- Upgrade device from PC using "PC_XXXX.s19" file
- Upgrade device from Pocket PC using "PPC_XXXX.s19" file
WARNING:
Use of the incompatible version
of firmware will cause the device to fail.
The PC and Pocket PC firmware download files are not interchangeable. |
Step 4 of 4
To install firmware in the UDC 2500, follow the directions outlined in the PIE
Download Instructions manual included in the Download file in Step 2.
Firmware History
|