|
|||||||||||||||||
Oxidation Reduction Potential Measurement for Microbiological Control in Makeup Water and Cooling Water
Background
|
|
|
The Problem
Historically, micro- and macroorganisms in water have been controlled by adding an oxidizing biocide such as chlorine, bromine, or ozone to effectively limit microbial activity. Laboratory screening procedures are coupled with maintaining a residual level of the biocide to ensure the maximum "kill" rate. This method has typically resulted in a periodic underfeed, leading to organism growth, or overfeed, adding unneeded expense and potential component damage. In contrast, the measurement of oxidation reduction potential (ORP) has proven more effective in consistently controlling biocide addition while effectively destroying the organisms, maximizing cost savings and component life.
Oxidizing Microbiocides
Chlorine
Equation 1: Cl2 + H2O ---> HOCl + HCl In addition to the above reaction, hypochlorous acid will ionize according to the following reversible reaction: Equation 2: HOCl ---> H+ + OCl- The effectiveness of chlorine as a biocide (known as the biocidal efficacy) is determined by the amount of hypochlorous acid, not the hypochlorite ion. Hypochlorous acid is a very strong oxidizing agent. It inhibits a cell's protein production and respiration processes, effectively destroying the cell. However, the pH of the water directly affects ionization of the hypochlorous acid. At a pH of approximately 6.0, only 5% of the hypochlorous acid ionizes to form the hypochlorite ion, while a pH of 7.0 yields ionization of around 25%. At pH 8.0, about 75% of the ionization occurs. The effectiveness of chlorine as an oxidizing agent is limited to pH levels below 8.0 pH. A pH range of 6.5 to 8.0 is considered the practical range for the use of chlorine as an oxidizing microbiocide, since lower pH levels can cause corrosion of piping, while higher pH levels render the chlorine ineffective. Although chlorine is widely used as an oxidizing agent, it has many inherent environmental, health, and safety concerns associated with it. The major disadvantage of chlorine use is the formation of chlorinated organics in the water, which can have a negative effect on the environment and process components. Another disadvantage of chlorine is potential safety problems associated with chlorine gas. In addition, chlorine tends to react with ammonia or nitrogen when they are present in the water, forming chloramines, which are believed to be harmful to the environment. Formation of chloramines requires the addition of excess chlorine to effectively disinfect the water, since chloramines reduce the effectiveness of the hypochlorous acid, thus wasting the chlorine. Chlorine addition also effectively lowers the pH of the water as hydrochloric and hypochlorous acids form, making pH control more difficult. As a result of the many problems associated with chlorine, many other oxidants are seeing more widespread use.
Bromine
Equation 3: Br2 + H2O ---> HOBr + HBr
Equation 4: HOBr
---> H2 + OBr-
Hypobromous acid is also a very strong oxidizing agent and acts to disrupt
the protein production and respiration processes of a cell. There are many
benefits to bromine over chlorine. However, t, however. The ionization of
hypobromous acid does not occur until much higher pH levels than those
needed for the ionization of hypochlorous acid. A pH of 8.0, which would
yield about 75% ionization of hypochlorous acid, yields ionization of only
slightly less than 20% of the hypobromous acid. A pH level of 9.0 must be
reached before the ionization of hypobromous reaches 75%. Bromine addition
is thus more useful in systems that maintain higher pH levels. Similarly to
chlorine, bromine will react with ammonia and nitrogen to form bromamines.
However, bromamines are considerably more powerful disinfectants than the
associated chloramines, so additional bromine is not necessary to
compensate, as with chlorine. The corrosive effect on process components
are lessened as well with bromine, since hypobromous acid is not as
powerful as hypochlorous acid. The environmental issues associated with
chlorine are also minimized with bromine. For these reasons, bromine use
has seen a significant increase as plants seek to minimize the problems
associated with chlorine while maintaining the oxidizing power needed to
prevent organism growth.
Sodium Hypochlorite
Equation 5: NaOCl + H2O
---> HOCl + NaOH
Sodium hypochlorite is considered safer to handle and ship than chlorine,
and thus may be preferred for these reasons. However, it is slow to
decompose and has adverse reactions with ammonia and organics. pH control
can be more difficult because of the formation of sodium hydroxide, a
strong base. In applications like cooling towers, where higher pH levels
are typically desired, sodium hypochlorite may be preferred over chlorine
addition, which will lower the pH levels.
Chlorine Dioxide
Ozone
ORP and Microbiocide Control
Control by means of the residual method has many shortcomings. The
concentration units used to report residual levels do not provide an
adequate representation of the quantity of organics that will be oxidized.
This is because an amount of oxidant will always oxidize the same number of
microorganisms, regardless of the concentration level. Another shortcoming
is that the oxidizing ability of the oxidant is often related to the pH of
the water. The residual measurement cannot take into account the pH, and
therefore fluctuations in the water pH will affect the ability of a
measured amount of oxidant to do its job. Another problem with residual
measurement is that some oxidants can exist in many forms in the water, and
residual measurements cannot take into account any changes within the
amounts of the various forms (all with varying oxidizing power) within the
water. Last of all, residual control has little ability to respond to
changes in demand, which can occur from fluctuating organic levels and
nitrogen compound levels, as well as any effects of flow, heat, light, or
exposure to air. In fact, when demand increases, oxidant strength will
diminish, although this effect may not be noted by residual measurements.
As a result, control of the addition of an oxidant by residual control
will result in endless overfeed and underfeed of the oxidant.
This overfeed/underfeed situation will cause two problems to occur. An
overfeed of oxidant will result in extreme excesses of chemical costs as
well as potential damage to system components and metallurgy. An underfeed
of oxidant will result in potentially irreversible damage and loss of
efficiency due to microorganism growth. Both problems should be avoided at
all costs, yet the only way to improve residual control is to increase the
periodic checks in plate counts and perform more adjustments to the
setpoints of the residual control. This method can yield only slightly
better results, but will waste time, money, and energy in performing the
often daily checks that are required. In cases where the oxidizing agents
must be removed from the water (typically known as
"dechlorination" when chlorine is used), the same problems exist.
ORP can be used to perform accurate control of oxidant feed. The ORP value
is a direct reading of the activity of the oxidizing and reducing agents in
the water as they correspond to oxidation-reduction reactions. Research
shows that a microorganism's ability to survive in water is mainly
influenced by the ORP of the water. This is because the action of an
oxidizing microbiocide is to remove electrons from an organism, effectively
destroying certain processes that keep the organism alive. Since this
transfer of electrons is an oxidation-reduction reaction, ORP gives a
direct correlation of the ability of the water to prevent microbiological
growth.
ORP measurement uses an inert metal (typically platinum) measuring
electrode that detects a millivolt potential due to the transfer of
electrons within the process. The polarity and strength of the millivolt
potential created is dependent upon the levels of oxidizing and reducing
agents in the water. The millivolt potential is established on the
measuring electrode with respect to a reference electrode, which is similar
to that used in pH measurements. The typical reference electrode is the
silver/silver chloride (Ag/AgCl) electrode, although a saturated calomel
electrode has been used on occasion. Millivolt values are reported with
respect to one or the other, depending on which is used, and care must be
taken not to interchange the two, as millivolt differentials will exist.
In an oxidizing environment, caused by the presence of an oxidizing
microbiocide, a higher ORP will exist, while a lower ORP will exist in a
reducing environment. It is important to note that the actual crossover
point between water being oxidizing or reducing is dependent upon the
reference electrode. This point is typically somewhere between +200 to +250
mV, depending upon whether the Ag/AgCl or the calomel electrode is used and,
to a lesser extent, the temperature and oxygen content of the water.
Whereas residual measurements simply respond to the concentration of excess
oxidant that exists, ORP responds directly to the oxidant's toxicity to the
organisms. For each individual site and application, an ORP value must be
established based upon laboratory tests for organism growth. The control
setpoint will typically be the optimal ORP value that, when maintained,
will consistently prevent growth of microorganisms at the minimal dosage of
oxidant required. Any costs associated with maintenance for the measurement
are minimal compared with the cost-savings associated with the improved
biocide control.
Cooling Water
Microorganisms such as algae, fungi, or bacteria can enter a cooling water
system through the incoming water or through the air itself if a cooling
tower is present. In fact, a cooling water system can provide optimum
conditions for growth, since temperature and pH ranges are usually ideal,
and nutrients such as sunlight, organic matter, and inorganic salts are
found in abundance.
The effects of the microorganisms vary widely. Algae growth will result in
oxygen production, which can accelerate the corrosion reaction. Some forms
of algae are responsible for the accelerated deterioration of nitrite-based
corrosion inhibitors. Other types are known to cause silica fouling. Dead
algae will collect in the water, increasing the suspended solids, which can
cause fouling, providing food that will enhance bacterial growth, as well
as absorbing microbiocides, which can minimize the effectiveness of
microbiological control. Fungi growing in a cooling tower can attack the
wood, causing surface rot or internal wood decay, which ultimately can
destroy a tower. Fungus growth can form bacteria-like slimes that can clog
heat exchange tubes, lowering the efficiency of the heat exchanger, as well
as causing site-specific corrosion whenever the slimes cling to pipe walls.
Minimizing bacteria growth is perhaps the most difficult microbiological
control, since so many different species of bacteria can exist in cooling
water systems. Problems associated with bacteria are perhaps the most
widespread of all the microbial concerns. Slimes can form that clog heat
exchangers. Some aerobic bacteria form strong acids, which can lower the pH
of the water in general, as well as locally dropping pH levels to as low as
1.0. Typically, anaerobic bacteria can grow underneath the aerobic
bacteria, causing site corrosion. "Iron" bacteria can produce
iron deposits that cause plugging, pitting corrosion, and reduced heat
transfer. Certain types of bacteria can destroy nitrite corrosion
inhibitors. Other bacteria can form ammonia, which can attack copper-based
construction materials. Safety issues can also arise from bacteria forms
known as pneumonia, including the Legionella pneumophila, which can cause
Legionnaires' disease.
Many cooling systems use fresh water as the intake water, which can
introduce numerous forms of macrofouling, such as clogging of filters or
screens. Large aquatic organisms can enter the water supply, causing
plugging in heat exchangers and buildup in a cooling tower basin. These
organisms include barnacles, clams, jellyfish, and mussels.
Microbiological growth in a cooling water system is typically controlled by
addition of chlorine, although sodium hypochlorite, bromine, chlorine
dioxide, and ozone are becoming more common as their benefits are realized.
Underfeed of the biocide will result in microbiological growth, while
overfeed of the biocide can result in excess chemical costs and potential
damage to the system metallurgy (corrosion) or the cooling tower (wood
delignification). Oxidation-reduction potential can be used to correct the
underfeed and overfeed problems by providing a measurement of the minimum
amount of biocide addition necessary to prevent microbial growth.
ORP control can be implemented with a feedback loop, with the sensor placed
either before or after the heat exchanger, although a location after may be
better to ensure compensation for any drop in oxidant levels within the
heat exchanger. Determination of the ORP control setpoint must be done for
each individual site, since there will be many variations between sites,
including organism type, water chemistry, temperature, and oxidant type.
For the most part, control setpoints for oxidizing biocide addition will be
within the +550 to +650 mV range.
Dechlorination (or a similar removal of another type of oxidizing biocide
from the water) for environmental protection typically is done by addition
of a reducing agent, such as sodium bisulfite or sulfur dioxide, in order
to properly reduce the oxidant, such as chlorine or bromine. Since regular
water with no oxidizing or reducing agents present (except oxygen, which is
a mild oxidizer) will result in a reading of approximately +200 mV with the
Ag/AgCl electrode, an ORP of less than this value means that the
environment is reducing. Research has shown that addition of enough sulfur
dioxide or sodium bisulfite to provide an ORP value of just below +200 mV
will result in the reduction of the oxidant. Not all oxidants require this
procedure, since some, such as ozone, will break down quickly on their own.
Control of microbiological growth is not an option for the vast majority of
cooling water systems. Inadequate control has resulted in shortened
component life, loss of efficiency, and wasted chemical costs. Yet
microbiological control remains one of the most misunderstood and thus
neglected parts of a chemical treatment program for cooling water.
Measurement of ORP offers major improvements over treatment programs using
residual control of an oxidizing microbiocide, resulting in improved life
for heat exchangers and cooling towers, minimal usage of treatment
chemicals for chlorinating and dechlorinating, and increased efficiency of
plant processes that utilize the cooling water for heat exchange purposes.
Makeup Water
The effect of biological growth on makeup water can be significant. A
typical makeup water system (Figure 2) will perform biocide treatment to
the raw water upon entrance to the makeup system. The typical oxidant used
is chlorine, although sodium hypochlorite is finding more widespread use in
smaller systems. The chlorination is done as early as possible in order to
immediately reduce the organic growth to acceptable limits. A large
residual is typically maintained as long as possible in order to discourage
any further growth. This process is called hyperchlorination.
Unfortunately, the amount of oxidant feed necessary can shift often
according to changes in flow, raw water organism content, or even varying
oxidant levels already present if the raw water is from a municipality.
Another application in the system where oxidant addition has been seen to
be useful is in the removal of iron and manganese, which can form mineral
deposits on pipe walls and process components, lowering the makeup water
system's effectiveness. Aeration can be used to remove these mineral
contaminants, since contact with oxygen can cause them to form insoluble
compounds that can be removed by filtration, coagulation, or flocculation.
However, the oxidative reaction that takes place using aeration is rather
slow. An oxidant such as potassium permanganate or chlorine in conjunction
with a filter bed of greensand (a zeolite containing manganese) can serve
to speed up the oxidative process. Although this process requires constant
addition of the oxidant and periodic bed regeneration, it is preferable to
allowing a reduction in component efficiency due to iron or manganese
deposits.
Unfortunately, the oxidants that can prevent so many problems early on in
the makeup water process can actually be harmful later on. The presence of
a strong oxidizer such as chlorine can degrade ion-exchange resins,
resulting in more frequent regenerations, which can be costly. In addition,
reverse-osmosis systems are typically very susceptible to water treated
with chlorine and quickly degrade upon exposure. For these reasons, the
makeup water must be dechlorinated prior to any reverse-osmosis or
ion-exchange units in the system. There are typically two ways to
accomplish thisactivated carbon beds or chemical injection with
sulfur dioxide (SO2) or sodium bisulfite (NaHSO3).
Activated carbon beds can actually serve two purposes within a makeup water
systemto dechlorinate the water and to adsorb any organics that
remain in the water. The efficiency of the carbon beds in removing the
chlorine depends upon a number of things, including pH, temperature, and
organic load in the water. Unfortunately, carbon beds can become a
nurturing environment for organic growth and therefore need to be sanitized
often. The pH levels necessary for the carbon beds to effectively
dechlorinate can often be harmful to components downstream. In addition,
carbon fines can be released from the bed, causing problems downstream with
other components. Because of the number of problems associated with carbon
beds, many makeup water system are employing chemical injection to
dechlorinate and using special anion-exchange resins for removal of
organics.
Dechlorination by means of chemical injection involves adding a reducing
agent such as sulfur dioxide or a form of bisulfite, such as sodium
bisulfite. The bisulfite (or sulfur dioxide) is oxidized and the chlorine
reduced, thus removing the harmful effects of chlorine in the water. The
bisulfite ions are converted to sulfate ions, which are removed in the
anion exchanger. The chlorine ions are converted to chloride ions, which
are also removed by the anion exchanger. Failure to completely dechlorinate
can result in hydrolytic destruction of a polyamide reverse-osmosis unit or
damage to ion-exchange resins. However, overfeed of the reducing agent can
result in unneeded chemical costs and increased anion-exchange resin
regeneration.
Oxidation-reduction potential can successfully be used for both oxidant
addition and removal in makeup water. An ORP feedback loop can be placed
into the system loop where oxidant addition is required (typically at the
raw water inlet point). A second ORP feedback loop can be added just prior
to the reverse-osmosis or ion-exchange systems in the makeup water system.
Typical control points are site-specific, but typically reside within the
+600 mV range or higher for oxidant addition and +200 mV or lower for
oxidant removal. Control points should be determined by lab analysis for
microbiological activity and level of oxidant present.
In order to provide quality water for many plants with minimal costs, the
efficiency of makeup water components is vital. Control of micro- and
macroorganisms, both at the initial intake of raw water and throughout
parts of the system, is important to maximize component life. Inadequate
control can result in increased regeneration or permanent destruction of
vital components, loss of efficiency, and wasted chemical costs. Control by
ORP has shown major improvements over treatment programs employing residual
control of an oxidizing microbiocide, resulting in improved life for
ion-exchange resins and reverse-osmosis systems, minimal usage of
treatment chemicals for chlorinating and dechlorinating, and increased
efficiency of plant processes that use the makeup water.
Honeywell's ORP Measurement and Control Solution
ORP Probes
Features and benefits of the ORP probes:
ORP Analyzers
The 9782 series ORP
analyzer was designed to be the easiest analyzer to use while providing
you with the widest selection of advanced features:
Honeywells 7096 ORP analyzer
offers basic, economical pH/ORP measurement and control. The analyzer
ensures accurate and reliable pH/ORP measurements, while the ¼-DIN, NEMA 4
front-panel design makes the analyzer ideal for OEM applications where
panel space is limited.
Additional features of the 7096 pH/ORP analyzer:
|
|
|
|
|
|
[HOME] [Product Search] [Contact Us] [Top of Page]
|