|
|||||||||||||||||
Chrome Waste TreatmentMeasuring and Controlling pH and ORP Levels
Background
|
|
|
Chromates are used as corrosion inhibitors in cooling towers and in various metal-finishing applications, including bright dip, conversion coating, and chrome plating. The resulting wastewaters from rinse tanks, dumps, and cooling tower blowdown contain soluble chromium ion, Cr6+. This toxic ion must be removed before discharging the water into the environment, typically to a level less than 0.05 ppm. The most frequently used technique for chrome removal is a two-stage chemical treatment process. The first stage lowers the pH and adds reducing agents to convert the chrome from soluble Cr6+ to Cr 3+. The second stage neutralizes the wastewater, forming insoluble chromium hydroxide, which can be removed. For consistent treatment and stable control in this type of process, well-mixed reaction tanks with volume for adequate retention time are required, as shown in Figure 1. Retention time is calculated as the filled or usable tank volume divided by the waste flow rate and should typically be 10 minutes or more.
First Stage
2CrO3 + 3H2SO3 ---> Cr2(SO4 )3 +3H2O The first-stage reaction is monitored and controlled by two independent control loops: acid addition by pH control and reducing agent addition by ORP or oxidation-reduction potential control. These loops can often be handled with On-Off control using solenoid valves or metering pumps. The pH controller simply calls for additional acid whenever the pH rises above 2.5. The ORP controller calls for additional reducing agent whenever the redox potential rises above about +250 mV. (The + polarity is of the metal ORP electrode with respect to the reference electrode.)
The ORP titration curve, Figure 2, shows the entire millivolt range if Cr6+ chrome is treated as a batch. With continuous treatment, operation is maintained in the completely reduced portion of the curve near the +250 mV setpoint. The ORP setpoint can vary from installation to installation, depending on pH, reducing agent, presence of additional contaminants and dissolved oxygen, and the type of reference electrode. The exact setpoint for a given installation should be determined empirically at a potential where all the Cr6+ has been reduced, but without excess sulfite consumption, which can release sulfur dioxide gas. This point can be verified with a sensitive colorimetric test kit or similar check. Chrome reduction is slow; 10 to 15 minutes may be required for a complete reaction. This time increases if the pH is controlled at higher levels. Variation of pH also has a direct effect on the ORP, as shown in Figure 2. Thus pH must be closely controlled to achieve consistent ORP control.
Second Stage
Cr2(SO4)3 + 6 NaOH ---> 3 Na2SO4 + 2 Cr(OH)3 pH control in the second stage is more difficult than in the first, since the control point is closer to the sensitive neutral area. Although this reaction is fast, retention time of at least 10 minutes is usually needed for continuous treatment to achieve stability. Proportional pH control is often required in this stage. A subsequent settling tank and/or filter removes the suspended chromium hydroxide. Flocculating agents have been found helpful in this separation.
Batch Treatment
ORP Measurement
ORP is a measurement of the status of an oxidation-reduction reaction. The platinum or gold electrode detects the solution's ability to accept or donate electrons. A reducing ion (sulfite) provides electrons and tends to make the electrode more negative. An oxidizing ion (Cr6+) accepts electrons and tends to make the electrode more positive. The net electrode potential is related to the ratio of concentrations of the reducing and oxidizing ions in the solution. It is extremely sensitive in measuring the degree of treatment in the reaction tank. However, it cannot be related to a definite concentration of chrome and therefore cannot be used as a final effluent monitor of chrome concentration. Reliable ORP measurement requires a very clean metal electrode surface. Routine cleaning of electrodes with a soft cloth, dilute acids, and/or cleaning agents is recommended to promote fast response. Control at low pH levels in the first stage of treatment has also been found to help maintain clean ORP electrodes. Recommended Honeywell Equipment For Reduction: 7777 Durafet or Meredian pH Electrode Assembly 7082 pH Analyzer 7777 Meredian ORP Electrode Assembly Alternative for Reduction: 7773 pH and ORP Electrode Assembly Glass pH Electrode ORP Electrode (platinum) Terminal (p/n 31316441) 7082 Simultaneous pH/ORP Analyzer For Neutralization: 7777 Durafet or Meredian pH Electrode Assembly |
|
|
|
|
|
[HOME] [Product Search] [Contact Us] [Top of Page]
|