|
[A] [B]
[C] [D]
[E] [F]
[G] [H]
[I] [J]
[K] [L]
[M] [N]
[O] [P]
[Q] [R]
[S] [T]
[U] [V]
[W] [X]
[Y] [Z]
Absolute Pressure Sensor-a sensor
which measures input pressure in relation to zero pressure (a total vacuum
on one side of the diaphragm).
Actuator-mechanism of the switch or switch
enclosure which operates the contacts.
Acceleration-the rate of change of velocity.
Acceleration has two characteristics: magnitude and direction.
Accuracy- a comparison of the actual output
signal of a device to the true value of the input pressure. The various errors
(such as linearity, hysteresis, repeatability and temperature shift)* attributing
to the accuracy of a device are usually expressed as a percent of full scale
output (Span)
Alignment-placing the emitter (light source)
and receiver (photoreceiver or reflector) so as to direct the maximum amount
of light on the photosensor. At long distances, when the light beam has widened,
the receiver should be centered in the beam to lessen the chance of the emitter
and receiver drifting out of alignment due to vibration or shock.
Alternating Current (AC)-one that
reverses at regularly recurring intervals of time and has alternately positive
and negative values.
Ambient-in the area. 1) light-Light in the area
of the photosensor, but not originating with the control light source. Ambient
light can adversely affect non-modulated control operation, and should be
screened, if possible, from the sensor; 2) Temperature-average temperature
of surrounding medium such as water, air, or earth, into which the heat of
the equipment is dissipated.
Analog Output-having the property of being
continuously variable, as opposed to having discrete states.
AND Logic-an output is produced only when all
inputs are present.
Analog Output- an electrical output from
a sensor that changes proportionately with any change in input pressure.
Anode-the switch contact connected to the positive
terminal of the power supply.
Aperture-most often an external cap (with a
small opening) placed over the receiver lens to help detect small objects.
It lets even a small object block enough light to be detected. Also, an internal
aperture in most receivers reduces the effect of off-axis ambient light.
Arc-one of several kinds of visible electrical discharge
between separated contacts of a switch. It is primarily a stream of electrons
and is accompanied by incandescent metal vapor.
Attenuation-loss or reduction of beam intensity
as a result of environmental factors, dust, humidity, steam etc.
Auto Zeroing Technique- a method used to
automatically set the null point on a pressure sensor. This is usually done
by using a microprocessor to open a solenoid valve at a predetermined time
interval. This references atmospheric pressure to both sides of the pressure
sensor chip. The microprocessor reads the output voltage and makes that the
new null point. This method is used to eliminate errors due to null offset
and null temperature shift.
Auxiliary Actuator-a mechanism, sold
separately, to provide basic switches with easier means of operation and
adjustment and adapt switches to different operating motions by supplying
supplemental overtravel.
[Top of page]
Basic Switch-a self contained switching
unit. It can be used alone, gang-mounted, built into assemblies or enclosed
in metal housings.
Bifurcated Contact-a movable or
stationary contact which is forked or divided to provide two pairs of mating
contact surfaces connected in parallel, instead of a single pair of mating
surfaces.
Bidirectional Differential Pressure
Sensor-a differential pressure sensor allowing the greater input
pressure to be applied to either pressure port.
B.F.S.L. (Best Fit Straight Line)-a method for
defining linearity. A straight line placed on a sensor output curve such
that half the data points lie above and half below that line. The method
for determining B.F.S.L., is the sum of least squares.
Bridge Resistance- see Input Impedance
and Output Impedance.
Break-to open an electrical circuit.
Break Distance-the minimum distance between
separated mating contacts in their fully open position.
Burst pressure-the specified pressure
which will rupture the sensing element but not the sensor case.
[Top of page]
Cascade-to combine logic circuitry to get more
complex logic or timing control. (Inputs and outputs are wired in series.)
Calibration-a test during which known values
of Measurand are applied to the device under test and corresponding
output readings are recorded under specified conditions.
Calibration Curve-a graphical
representation of the calibration record.
Calibration Cycle-the application of
known values of Measurand and recording of corresponding Output readings
over the full or the specified portion of the Range, in an ascending and
descending direction.
Catalyst-a substance which changes the rate
of a chemical reaction but is itself not changed. Switch contact material
sometimes acts as a catalyst, accelerating the formation of polymers on the
contact surface.
Cathode-the switch contact connected to the
negative terminal of the power supply.
Characteristics-This term is used by
MICRO SWITCH in a restricted sense and refers only to switch operating
characteristics such as pretravel, operating force, etc.
Clean Air-ideal conditions. Climate controlled
or sterile area.
Chip-a die (unpackaged semiconductor device) cut
from a silicon wafer, incorporating semiconductor circuit elements such as
resistors, diodes, transistors, and/or capacitors.
Compensation-procedure of providing a
supplemental device, circuit, or special materials to conunteract known sources
of error (e.g., ambient temperature change). Compensation is often related
to temperature compensation only.
Complementary Output-both N.O. and
N.C. outputs are available for use. A circuit that provides sink or source
capability with a single input. Output that can be both light operated and
dark operated. (Also known as 4-wire DC controls.)
Control-the complete system; sensor, amplifier,
output.
Control Base-unit remote from sensor in
which amplification and conditioning of the input signal takes place. Usually
contains a power supply and an output device.
Convergent Beam-A variation of the diffuse
scanning mode. A photoelectric control whose optical system is key to its
operation. It simultaneously focuses and converges a very small, intense
beam to a fixed-focal point in front of the control. The control is essentially
blind a short distance before and beyond this focal point. Convergent beam
scanning is used to detect the presence or absence of small objects while
ignoring nearby background surfaces.
Convertible Output-output that can
be wired either as Normally Open or Normally Closed, but not at the same
time.
Corrective Factor-the mathematical
factor that, when multiplied by the sensing distance of a given sensor, will
adjust sensing distance for the different metals being used as targets.
Current-time value of movement of free electrons.
One ampere equals one coulomb per second. Conventional reference is opposite
to direction of actual electron movement.
Current Consumption-the amount of
current required to power a sensor or control (excluding load). See
supply current.
Current Sinking-an output type such that
when it is On, current flow is from the load into the device's output, then
to ground. Output is Normally High. The sensor "sinks" current from the load
through the sensor to ground. The load is connected between the positive
lead of the supply and the output lead of the sensor.
Current Sourcing-an output type such
that when it is On, current flow is from the device into the load. Output
is Normally Low. The sensor "sources" current to the load. The load is connected
between the output lead and the negative ground lead of the supply.
[Top of page]
Dark Operated (D.O.)-control operating
mode in which the output (load) is energized when the light is blocked
(retro/thru scan) or object not present (diffuse), the photosensor is dark.
Dead Break-Imperfect snap action in which
the normally closed circuit of the switch opens before the plunger reaches
the operating point, or the normally open circuit opens before the plunger
reaches the release point.
Dead Make-Imperfect snap action in which a
switch fails to close its circuit when the plunger reaches the operating
or release point.
Diaphragm-the membrane of material that remains
after etching a cavity into the silicon sensing chip. changes in input pressure
cause the diaphragm to deflect.
Dielectric-the term dielectric is almost
synonymous with electrical insulation, which can be considered the applied
form of the dielectric.
Dielectric Breakdown-rupture of
insulation material when the electric stress exceeds the dielectric strength
of the material.
Dielectric Strength-the maximum potential
gradient that a material can withstand without rupture. As a material property
it usually is calculated by dividing the breakdown voltage by the thickness
of the material between a pair of test electrodes. The term often is applied
to switches to mean the maximum voltage a switch can withstand between specified
terminals or between terminals and ground without leakage current exceeding
a specified value.
Differential Pressure Sensor-a
sensor which is designed to accept simultaneously two independent pressure
sources. The output is proportional to the pressure difference between the
two sources.
Differential Travel-the distance
from the operating point to the release point.
Diffusion-a thermochemical process whereby
controlled impurities are introduced into the silicon to define the
piezoresistors. Compared to ion implantation, it has two major disadvantages:
1) the maximum impurity concentration occurs at the surface of the silicon
rendering it subject to surface contamination, and making it nearly impossible
to produce buried piezoresistors; 2) control over impurity concentrations
and levels is about one thousand times poorer than obtained with ion
implantation.
Diffuse Scan-a reflective scanning technique
in which reflection from a near-by non-shiny surface illuminates the photosensor
in the receiver. Sometimes called proximity scan because of the required
nearness of the light source and photosensor to reflecting surface. Also
used to detect color contrast as in registration control.
Digital Circuit-a circuit that has only
two stable states, operating in the manner of a switch; that is, it is either
On or Off.
Digital Output-output that is of only
two stable states, appearing in the manner of a switch; that is, it is either
On or Off or High or Low (i.e., high voltage or low voltage).
Direct Current (DC)-a unidirectional current
in which changes in value are so small that they may be neglected. As ordinarily
used, the term designates a practically non-pulsating current.
Direct Scan-see
thru scan.
Disable-to prevent the output despite an input
signal. A wiring terminal for this purpose is provided on most MICRO SWITCH
control bases. The disabling circuit may receive its signal from the current
sinking output of a photoelectric logic card, or modulated LED control, or
from an electromechanical limit switch, etc. Disabling is used to prevent
false or unwanted signals from triggering the control.
Double Break Contacts-(Twin break).
This breaks the circuit in two places. Referred to as form Z circuitry also.
Double-Pole Double Throw
(DPDT)-switches which make and break two separate circuits. This
circuit provides a normally open and normally closed contact for each pole.
Drift-an undesired change in output over a period
of time, which is not a function of any input pressure change.
Drift of an Operating
Characteristic-an inexact term referring in a general way to the
degree of instability of a plunger force or travel characteristic under specified
conditions and during a specified number of cycles of switch operation.
Dry Circuit-slang expression meaning a low
energy circuit. Although many individuals and groups have assigned current
and voltage values to "dry circuits" there is at present no general agreement
as to what the values should be.
[Top of page]
Effective Sensing Distance-the
difference between nominal sensing distance and the % manufacturing tolerance.
Electrical Life-life of a switch under
a specified combination of electrical load, actuation, environment and criterion
of failure. Synonymous with switch life.
Enable-the opposite of disable. To allow output
in response to an input signal. We often speak of one light source-photoreceiver
pair (the "gating" pair) enabling a second pair (the "inspect" pair).
Enclosed Switch-a basic switch unit (contact
block) enclosed in a durable metal housing. The enclosure protects the switching
unit, provides mounting means, and fitting for conduit
connection.
End points-the Outputs at the specified upper
and lower limits of the Range.
Environment-Proof Switch-a switch which
is completely sealed to ensure constant operating characteristics. Sealing
normally includes and "O" ring on actuator shaft and fused glass-to-metal
terminal seals or complete potting and an elastomer plunger-case seal.
Erosion, Contact-a general loss of material
from one or both working surfaces of a pair of mating contacts, as a result
of switching an electrical load.
Error-the algebraic difference between the indicated
value and the true value of the input pressure. Usually expressed in percent
of full scale output, sometimes expressed in percent of the sensor output
reading.
Error Band-the band of maximum deviations
of the output values from a specified reference line or curve due to those
causes attributable to the sensor. Usually expressed as "+ -% of full scale
output." The error band should be specified as applicable over at least two
calibration cycles, so as to include repeatability, and verified accordingly.
Excess Gain-the ratio of optical power available
at a given emitter-to-receiver range to the minimum optical power required
to trigger the receiver.
Excitation-the external source of energy
(e.g., electrical voltage or current) applied to a sensor for its operation.
Explosion-Proof-having the ability to
contain an explosion within the sensor or housing if it were to occur.
Explosion-Proof Switch-a UL listed
switch capable of withstanding an internal explosion of a specified gas without
ignition of surrounding gases.
External Inhibit-see
disable.
Extreme Contamination-coal bins,
residue on lens.
[Top of page]
Fall Time-a measure of the time required for
the output voltage of a circuit to change from a high voltage level to a
low voltage level, once a level change has started (90% to 10%).
False Pulse-an improper change of state of
the output, usually associated with Turn-Off or Turn-On.
False Pulsing-circuitry designed to clamp
output Off until the power supply has time to reach proper voltage level.
Typically 200-500 msec.
False Pulse Protection-circuitry
designed to clamp output Off until the power supply has time to reach proper
voltage level. Typically 200-500 msec.
Fiber Optics-transparent fibers of glass
or plastic used for conducting and guiding light energy. Fiber optics are
used in photoelectrics as light pipes consisting of a bundle of small optical
fibers (glass) or single strand (plastic) housed inside a flexible sheathing.
Force, Contact-the force holding closed
contacts together.
Force Differential-the difference
between the operating force and the release force.
Free Position of the
Plunger-the position of the plunger when there is no external force
other than gravity applied to it.
Frequency, Natural-the frequency of
free (not forced) oscillations of the sensing element of a fully assembled
sensor.
Frequency Output-an output in the form
of frequency which varies as a function of the applied pressure.
Full Overtravel Force-the force
required to depress the plunger of a switch to the full overtravel point.
Full Overtravel Point-that position
of the plunger beyond which further overtravel would cause damage to the
switch or actuator.
Full Scale Output (Span)-the algebraic
difference between output curve end points (outputs at specified upper and
lower output limits).
[Top of page]
Gage Factor-a measure of the ration of the
relative change of resistance to the relative change in length of a resistive
strain sensor (strain gage).
Gage Pressure-a form of differential pressure
measurement in which atmospheric pressure is used as a reference.
Gravity Unit-one gravity unit (abbreviated
g) is an acceleration of 32.2 feet per second per second.
Ground-a conducting path, intentional or accidental,
between an electric circuit or equipment and the earth, or some large conducting
body serving in place of the earth (a voltage reference).
[Top of page]
Hall Effect Technology-the description
given to the following phenomena; when a semiconductor, through which a current
is flowing, is placed in a magnetic field, a difference in potential (voltage)
is generated between the two opposed edges of the conductor in the direction
mutually perpendicular to both the field and the conductor. Typically used
in sensing magnetic fields.
Hardwired-physically interconnected and intended
for a specific purpose. Hardwired logic is essentially unalterable.
Hazardous Location-defined as an area
in which flammable or combustible mixtures are present.
Head-On-a condition whereby the target approaches
the sensing face of the proximity sensor with its center along the sensing
face.
High Contamination-heavy particle
laden air, extreme washdown environments, grain elevators.
Hermetically Sealed Switch-a
switch completely sealed to provide constant operating characteristics. All
junctures made with metal-to-metal or glass-to-metal fusion.
Hysteresis, Switching-the principle
associated with sensors, such that the operate point is not at the same level
as the release point. In solid state sensors, it is accomplished electrically.
In mechanical switches, it results from the storing of potential energy before
the transition occurs. Also known as differential, and is usually expressed
as a percentage of the operate point (e.g. 3-15%).
[Top of page]
|