|
[A] [B]
[C] [D]
[E] [F]
[G] [H]
[I] [J]
[K] [L]
[M] [N]
[O] [P]
[Q] [R]
[S] [T]
[U] [V]
[W] [X]
[Y] [Z]
Immediate Response-control transfers
On/Off state immediately when target enters the detection range, and reverses
state immediately when target leaves detection range.
Inductive Technology-technology
based on inductance, the property of an electric circuit by which an
electromotive force is induced in it by a variation of current, either 1)
in the circuit itself, or 2) in a neighboring circuit.
Infrared (IR)-the invisible radiation (as opposed
to visible light) that certain LEDs emit. Standard MICRO SWITCH modulated
LED controls have infrared emitting LEDs.
Inhibit-see
disable.
Input-1) The device or collective set of devices
used for bringing data into another device; 2) The signal or stimulus put
into a circuit to make the output do something.
Input Impedance-the impedance (presented
to the excitation source) measured across the excitation terminals of a sensor.
Input Signal Duration-a length of
time the light beam is blocked (in dark operated mode), or uniterrupted (in
light operated mode). Or, the length of time a target is within the operating
range.
Insulation Resistance-the resistance
measured between specified insulated points on a sensor when a specified
DC potential is applied at room conditions.
Insulator-a non-conducting support for an
electric conductor. A material that does not conduct electricity.
Integrated Circuit (IC)-an interconnected
array of active and passive elements integrated within a single semiconductor
substrate or other compatible material, and capable of performing one complete
electronic function.
Interface-a common boundary between electronic
systems, or parts of a single system.
Interface Circuit-a circuit that links
one type of device with another. It's function is to produce the required
current and voltage levels for the next stage of circuitry from the previous
stage.
Interrogate (Gate)-a function usually
performed by gating light source-photoreceiver pair; asking (interrogating)
whether a certain condition has been met (for example, proper fill level
in boxes moving along a conveyor), and thereby enabling or disabling an inspect
light source-photoreceiver pair (which will count only full boxes).
Intrinsically Safe-limits
electrical/thermal energy to levels incapable of causing ignition. External
barriers are required.
IP-European environmental ratings similar to USA
NEMA ratings.
Ion Implantation-a process whereby impurity
ions are accelerated to a specific energy level and impinged upon the silicon
wafer. The energy level determines the depth to which the impurity ions penetrate
the silicon. Impingement time determines the impurity concentration. Thus,
it is possible to independently control these parameters, and buried
piezoresistors are easily produces. Ion implantation is increasingly used
throughout the semiconductor industry to provide a variety of products with
improved performance over those produced by diffusion.
IR-Infrared: A portion of the spectrum of light which
is not visible (wavelengths which extend beyond 770nm).
IRED-Infrared-Emitting Diode: a diode capable of
emitting radiant energy in the infrared region of the spectrum.
[Top of page]
[Top of page]
[Top of page]
Laser Trimming (Automated)-a method for
adjusting the value of thick film resistors using a computer-controlled laser
system.
Latching Logic-signal modification that
causes the output to be energized and remain energized (maintain output).
Latched output may be immediate or delayed. Usually, the latch is released
by closing a circuit between the reset (RS/D) terminal and ground.
Leakage Current-small current flowing
through or leaking from the output device in the Off state due to semiconductor
characteristics.
Leakage Rate-the maximum rate at which a
fluid is permitted or determined to leak through a seal. The type of fluid,
the deferential pressure across the seal, the direction of leakage, and the
location of the seal must be specified.
Least Squares Line-the straight line
for which the sum of the squares of the residuals (deviations) is minimized.
This method is used to calculate B.F.S.L. linearity.
LED (Light Emitting Diode)-a solid state light source
that emits variable light, or (in MICRO SWITCH modulated LED controls) invisible,
infrared radiation.
Light Operated (L.O.)-control operating
mode in which the output is energized when the light beam is not blocked
(retro/thru scan), or object is present (diffuse) the photosensor is illuminated.
Linearity (Linearity Error)-the deviation
of the sensor output curve from a specified straight line. Linearity error
is usually expressed as a percent of full scale output.
Linearity (End Point)-see Terminal
Base Linearity
Linear (Output)-output that is a continuous
amplified version of its input. That is, the output is a predetermined variation
of its input.
Linearity (Terminal Base)-see
Terminal Base Linearity.
Load Current-units = Amps/milliamps (DC)
or Amps RMS/milliamps RMS (AC). The maximum amount of current that a proximity
sensor will switch through its load. Load current for a particular device
can be calculated by dividing the load voltage by the load resistance. Attempting
to switch a higher load current than the sensor is rated for will result
in sensor failure.
Load Impedance-the impedance presented
to the output terminals of a sensor by the associated external circuitry.
Logic-the modification of an input signal that
produces delayed, pulsed, latched. or other output response. Logic circuitry
is sometimes an integral part of the control, but more often, a separate
plug-in card or module.
Low Contamination-warehouse locations,
light industry applications, material handling operations.
Low Energy Circuit-a qualitative term
having no exact definition. It usually refers to a circuit having such low
voltage and current that there are no significant thermal effects at the
contact interface.
[Top of page]
Magnetic Blow-Out Switch-contains
a small permanent magnet which provides a means of switching high DC loads.
The magnet deflects arc to quench it.
Maintained Contact
Switch-designed for applications requiring sustained contact after
plunger has been released, but with provision for resetting.
Manufacturer's Tolerance-the
maximum variation from standard allowed by the manufacturer between products
with the same catalog listing.
Make-to close or establish an electrical circuit.
Maximum Excitation-the maximum value
of supply voltage or current that can be applied to the sensor at room conditions
without causing damage or performance degradation beyond specified tolerances.
Maximum Load Current-the maximum
amount of current that can flow through a sensor and not cause sensor failure.
Measurand-a physical quantity, property or
condition which is measured (e.g., pressure, acceleration).
Mechanical Life-life of a switch with
no (or a negligible) electrical load, and a specified combination of actuation,
environment and criterion of failure. Mechanical life usually is limited
by the life of the switch's flexing parts and bearing surfaces.
Media compatibility-ability to operate
with a specified media carrying pressure (e.g., salt water).
Metalization-the metal pattern deposited
on the sensor chip (usually outside the diaphragm area) to permit electrical
connections to be made to the chip. Aluminum is usually used, but has potential
contamination problems (known as the "purple plague"), if not protected.
MICRO SWITCH uses gold, which is impervious to almost everything.
Migration, Contact Material-a
net transfer of material from one contact to the mating contact as a result
of switching an electrical load. It usually takes the form of a needle, cone
or mound or one contact face and a corresponding pit in the surface of the
mating contact.
Minimum Life-this is an exact term only
when applied to a specific group of tested switches. It then means the lowest
life figure obtained from the test of that group of switches.
Moderate Contamination-milling
operations, areas of high humidity, stream.
Modulated Light Source (MLS)
Control-a photoelectric control that operates on modulated (pulsed)
infrared radiation, and responds only to that frequency rather than steady
light intensity. Modulated LED controls offer a high rejection of troublesome
ambient light.
Momentary Short Circuit
Protection-output circuit protection designed to protect the output
device from damage due to a temporary (1-3 sec.) short circuit or until an
external fuse can interrupt current.
Momentary Short Circuit-a switch
with contacts that return from operated condition to normal condition when
actuating force is removed. Unless otherwise stated, all switches in this
catalog are momentary.
Momentary Switch-a switch with contacts
that return from operated condition to normal condition when actuating force
is removed. Unless otherwise stated, all switches in this catalog are momentary.
[Top of page]
NEMA Ratings-National Electrical Manufacturers
Association ratings of an enclosure's ability to provide a degree of protection
against contact with equipment and against specified environmental conditions.
Noise, Electrical-noise results from
the presence of undesirable electrical voltages or current. It causes devices
to operate erratically (if the noise is on the supply line to a device),
or produces false information on erratic operation if present on wires carrying
signals from the output of a device to the load. Noise can be present in
the supply or picked up on lines in many ways. Pick-up from noisy adjacent
wires or metal parts is possible. Good wiring practice and/or additional
parts can be used to diminish the effects of noise.
Nominal Sensing Distance-an
approximate dimension value measured from the face of the sensor to the nearest
point of the target. It does not take into consideration manufacturer's tolerance
or operational variables. Also known as the operating point.
Non-contact-a slang expression referring
to a defective condition in which a supposedly closed switch lacks electrical
continuity.
Nonincendive-inability under normal operation
to ignite a hazardous mixture.
Non-modulated Controls-controls
designed for indoor applications subject to neither bright ambient light
nor extreme vibration. Usually incandescent lamp controls, scanners and light
source-photoreceiver pairs.
Normal Contact Position-the normal
contact position of a switch exits when no force is applied to the plunger.
Normal High-the state of a control in which
the output is high (logic1) in voltage in the rest (Off) condition.
Normally Low-the state of a control in which
the output is low (logic 0) in voltage in the rest (Off) condition.
Normalization-process of creating sensor
interchangeability.
NPN-a transistor consisting of two N-type regions
separated by a P-type region.
Null-the condition when the pressure on each side
of the sensing diaphragm is equal.
Null Offset-the electrical output present,
when the pressure sensor is at null.
Null Temperature Shift-the change
in null output value due to a change in temperature.
[Top of page]
Off Delay Logic-adjustable delay (after
input signal stops) before output is de-energized.
Off State Current-the supply or bias
current flowing into a solid state device when it is in the unactuated state
(see Leakage Current).
Ohm-the unit of electrical resistance. Resistance
through which a current of one ampere will flow when a voltage of one volt
is applied.
On Delay Logic-adjustable delay (after
onset of input signal) before output is energized.
One-shot Logic-see
pulsed logic.
Opacity-the characteristic of an object that
prevents light from passing through. The opposite of translucent. Opaque
objects are easy to detect since they block light almost entirely.
Operated Contact Position-the
position to which the contacts move when the plunger is traveled to the operating
point or into the overtravel range.
Operating Characteristics of a
Switch-the commonly specified force, torque and linear or angular
travel properties of a switch. Examples: operating or release force, operating
point, differential, overtravel.
Operating Force-the force which must
be applied to the plunger to cause the moving contact to snap from the normal
contact position to the operated contact position.
Operating Mode-refers to the condition
of the photosensor (dark or light illuminated) that energizes output. A mode
selector switch determines the operating mode.
Operating Point-that position of the
plunger at which the contacts snap from the normal contact position to the
operated contact position.
Operating Temperature-actual range
over which sensors can be operated. Usage outside the temperature limits
will result in loss of stability, change in operate point and possible permanent
damage to the sensor. Nominal sensing distance is determined at 25 - C.
Optical Power-power or intensity of the
projected light available from a particular emitter; beam intensity.
OR Logic-an output is produced when any one
or more inputs are present.
Output-the useful energy delivered by a circuit
or device. Can mean energy produced at the output terminals of an amplifier-a
source of energy.
Output Impedance-the impedance across
the output terminals of a sensor presented by the sensor to the associated
external circuitry.
Output Noise-the rms, peak-to-peak (as
specified) AC component of a sensors DC output in the absence of a change
in input pressure.
Overpressure-the maximum specified pressure
which may be applied to the sensing element of a sensor without causing a
permanent change in the output characteristics.
Overtravel-as an operating characteristic
of a switch, overtravel is the distance through which the plunger moves when
traveled from the operating point to the full overtravel point. As a
characteristic of the actuation applied to the switch, overtravel is the
distance the plunger is driven past the operating point.
[Top of page]
Parallel Circuit-a circuit in which
current has two or more paths to follow. Two electrical elements are in parallel
if both terminals of both elements are electrically connected.
Photocell-a resistive, bulk effect type of
photosensor, the type used when it is desirable to wire several photoreceivers
in series or in parallel. The resistance decreases with increasing light
intensity.
Photoreceiver-a unit consisting of
photosensor, focusing lens, and protective enclosure.
Photosensor-a light sensitive portion of
a photoelectric control that converts a light signal into an electrical signal.
MICRO SWITCH uses photocells and phototransistors.
Phototransistor-a type of photosensor.
Typically used where speed of response is important or ambient temperature
variations are great.
Piezoresistance-a change in resistance
in a semiconductor, caused by an applied stress to the diaphragm.
Polarized Photoelectric
Controls-controls that emit a visible LED beam and use a special
lens which filters the beam of light so that it is projected in one plane
only. The control responds only to the de-polarized reflected light from
corner-cube type reflectors (FE-RR1) or special polarized reflective tape.
PN-a diode consisting of one N-type region and one
P-type region.
Pole-the number of completely separate circuits
that can pass through a switch at one time. A single pole switch can control
only one circuit at a time. A double pole switch can control two independent
circuits (such as a 120 volt AC heater and a 6 volt DC lamp) at the same
time. The number of poles is completely independent of the number of throws
and number of breaks.
Polymers Between
Contacts-compounds having long-chain molecular structure, formed
from simple organic contaminants on contacts, under the influence of contact
wipe and the catalytic effect of the contact material.
Power Dissipation-units = Watts/milliwatts
(DC) or Volt-Amps (AC). The amount of power that is consumed and converted
to heat in normal operation.
Supply Voltage (max) x Supply Current
(max) = Power Dissipation
Volts x Amps = Watts (DC) or Volt/
Amps (AC)
Precision Snap-Acting
Switch-an electromechanical switch having predetermined and accurately
controlled characteristics and having a spring loaded quick make and break
contact action.
Pressure-force applied to, or distributed over
a surface expressed in terms of force to area ratio.
Pressure, Absolute-pressure measured
relative to absolute zero pressure (perfect vacuum). The output of the absolute
sensor will change as a result of barometric pressure change. Thus it can
be used as a barometer.
Pressure, Differential-pressure
between two points of measurement.
Pressure, Gage-pressure measured relative
to ambient pressure. The output of a gage pressure sensor, contrasted to
an absolute pressure sensor, does not change with a change of barometric
pressure.
Pressure Range-the pressure limits over
which the pressure sensor is calibrated or specified.
Pressure, Reference-the pressure
relative to which a differential sensor measures pressure. Ambient pressure
is a specific case of reference pressure.
Pressure Sensor-a device that converts
an input pressure into an electrical output.
Pressure, Static-the average pressure
on the inputs of a differential pressure sensor (sometimes referred to as
common mode or working pressure).
Pretravel-the distance through which the plunger
moves when traveled from the free position to the operating point.
Proof Pressure-see Overpressure.
Proximity Scan-see
diffuse scan.
Proximity Sensor-a sensor with the ability
to detect the presence of a metal target, within a specified range, and without
making physical contact.
Pull-Down Resistor-a resistor connected
across the output of a device or circuit to hold the output equal to or less
than the zero input level. Also used to lower output impedance of digital
or analog devices. Usually connected to a negative voltage or ground.
Pull-Up Resistor-a resistor connected
across the output of a device or circuit to hold the output voltage equal
to or greater than the input transition level of a digital device. Usually
connected to the positive voltage or plus supply.
Pulse-a momentary sharp change in current, voltage,
or other quantity that is normally constant. A pulse is characterized by
a rise and fall and has a finite duration.
Pulsed Logic-a signal modification that
produces output independently of input signal duration. Pulse duration (dwell)
is usually adjustable. Also referred to as one-shot logic. Pulsed logic may
be immediate or delayed.
[Top of page]
|