|
[A] [B]
[C] [D]
[E] [F]
[G] [H]
[I] [J]
[K] [L]
[M] [N]
[O] [P]
[Q] [R]
[S] [T]
[U] [V]
[W] [X]
[Y] [Z]
Quiescent Supply Current-the
supply current being drawn when the pressure sensor is at null.
[Top of page]
Ratiometric (Ratiometricity Error)-at a
given supply voltage, sensor output is a proportion of that supply voltage.
Ratiometricity error is the change in this proportion resulting from any
change to the supply voltage. Usually expressed as a percent of full scale
output.
Range-the measurand values over which the sensor
is intended to measure, specified by the upper and lower limits.
Rectifier-a device that converts alternating
current into direct current.
Reed Technology-technology where the
reed contacts are designed to be actuated by a magnet. When a magnetic field
is brought close to the reed contacts, the contacts are drawn together to
make the circuit.
Reflective Scan-a scanning technique
in which the light source is aimed at a reflective surface to illuminate
the photosensor. Retroreflective, specular, diffuse scan and convergent beam
are all reflective scan techniques.
Regulation %-the ratio of voltage extremes
due to loading or line fluctuations. The process of holding constant a quantity
such as voltage by means of a system that automatically corrects errors.
For example, as more current is drawn from a battery or power supply, the
output voltage tends to decrease (load regulation). With a power supply derived
from AC, the DC output voltage can vary with the variation in AC voltage
(line regulation).
Release Force-the level to which force
on the plunger must be reduced to allow the contacts to snap from the operated
contact position to the normal contact position.
Release Point-that position of the plunger
at which the contacts snap from the operated contact position to the normal
contact position.
Release Travel-as an operating characteristic
of a switch, release travel is the distance through which the plunger moves
when traveled from the release point to the free position. As a characteristic
of the actuation applied to the switch, release travel is the distance the
plunger is released past the release point.
Repeatability-the ability of a sensor
to reproduce output readings when the same value is applied to it consecutively
in the same direction, for a specified number of cycles, or specified time
duration.
Resolution-the magnitude of output step changes
as the pressure is continuously varied over the range. This term applies
primarily to potentiometric sensors. Resolution is best specified as average
and maximum resolution. Usually expressed in percent of full scale output.
Response Time-the time it takes for a device
to respond to an input signal. The sum of the sensor, amplifier, and
output response is the total response time.
Retroreflective Scan-the reflective
scan technique that uses a special reflector (retroreflector) to return light
along the same path it was sent.
Reverse Polarity
Protection-circuitry, usually a diode which prevents current from
flowing into the control in case of accidental mis-wiring of the plus (+)
or minus (-) terminals, preventing damage to the unit.
Ripple-the alternating component of voltage from
a rectifier or generator. A slight fluctuation in the intensity of a steady
current.
Rise Time-a measure (10% to 90%) of the time
required for an output voltage to rise from a state of low voltage to a high
voltage level, once a level change has started.
Room Conditions-ambient environmental
conditions under which sensors must commonly operate, which have been established
as follows:
(a) Temperature: 25 + -10 %C (77 + - 18 degrees F).
(b) Relative humidity: 90% or less.
(c) Barometric pressure: 26 to 32 inches Hg.
Note: Tolerances closer than shown are frequently specified for sensor
calibration and test environments.
[Top of page]
Saturation Voltage-the voltage drop
appearing across a control device that is fully turned On.
Scan Technique-a method of scanning objects.
The two general categories are through and reflective scan.
Self-Contained Control-a photoelectric
control in which all three phases of control - sensing, signal conditioning,
and output - occur in a single device.
Self-Contained Sensor-a proximity
sensor in which all three phases of control, sensing, signal conditioning,
and output, occur in a single device.
Sensing Distance-the maximum recommended
distance between the sensor and standard target at which sensor will effectively
and reliably detect the target.
Sensing Element-that part of a sensor
which responds directly to changes in input pressure.
Sensitivity-maximum recommended distance
between the sensor and standard target at which sensor will effectively and
reliably detect the target.
Sensitivity Shift-a change in sensitivity
resulting from an environmental change such as temperature.
Sensor-a sensing element. The basic element that
usually changes some physical parameter to an electrical signal.
Series Circuit-a circuit in which current
has only one path to follow.
Shielded Sensor-a sensor which "senses"
only to the front of its face and ignores metals to its side. The presence
of such side metal, however, may cause a slight shift in operating
characteristics.
Signal Conditioning-to process the
form or mode of a signal so as to make it intelligible to or compatible with,
a given device, including such manipulation as pulse shaping, pulse clipping,
digitizing, and linearizing.
Signal Ratio-1) broadly, the comparison
of light seen by a photosensor when the beam is blocked to the light seen
when the beam is not blocked; 2) More specifically, the comparison of photocell
resistance when sensor is dark to when it is illuminated. Proper control
application involves establishing a large dark-to-light ratio.
Single-Pole Double-Throw
(SPDT)-switch which may either make or break a circuit, depending
on how it is wired.
Single-Pole Single-Throw
(SPST)-switch with only one moving and one stationary contact. Available
either normally open (N.O.) or normally closed (N.C.).
Shock, Mechanical-a short pulse of
acceleration, usually lasting only a few milliseconds. A typical shock test
pulse is a half-sine acceleration wave having 100g peak and .007 second duration.
Slide-By-the condition whereby the target
approaches the sensing face of the proximity sensor in such a direction that
its center will cross the axis of the sensing face at right angles.
Slight Contamination-indoor locations,
non-industrial areas, office buildings.
Snap Action-in strict terms, snap action
is a property of a switch such that the moving contact accelerates without
added travel of the plunger beyond that travel which was required to separate
the contacts. National Electrical Manufacturers Association defines snap
action as "a rapid motion of the contacts from one position to another position,
or their return. This action is relatively independent of the rate of travel
of the actuator." The word "relatively" is important. In actual fact, the
acceleration of the moving contact is partially dependent upon the velocity
of the plunger. The important point is that, once the plunger reaches the
operating or release point, the movable contact immediately transfers to
its opposite position without further travel of the plunger. A non-snap acting
switch lacks this feature.
Span-the algebraic difference between limits of
the pressure range.
Specular Scan-a reflective scan technique
in which reflection from a shiny surface illuminates the photosensor, which
must be precisely positioned to receive the reflected light. The angle of
incidence equals the angle of reflection.
Stability of an Operating
Characteristic-the extent to which an operating characteristic such
as operating point remains constant during a specified number of cycles of
switch operation, under specified conditions of actuation, electrical loading
and environment. Most clearly expressed as a graph of the characteristic
versus cycles of switch operation.
Standard Target-an object used for making
comparative measurements of operating distance. A square of mild steel, 1mm
thick. The length of the side of the square is equal to either:
A: the diameter of the circle inscribed on the active surface of the sensitive
face of the sensor, or
B: three times the rated operating distance, whichever is the greater.
Storage Temperature Range-the
minimum and maximum specified temperature which may be applied to the pressure
sensor without causing a permanent change in the output characteristics.
Strain Gage-a sensing device providing a
change in electrical resistance proportional to the level of applied stress.
Sublimation-the change of state of a materiel
from solid to vapor and back to solid without going through a liquid state.
Supply Current-units = Amps or milliamps.
The amount of current necessary to maintain operation of a photoelectric
control, proximity sensor or control base. Sometimes referred to as Current
Consumption.
Supply Voltage-units + Volts. The range
of power required to maintain proper operation of a photoelectric control,
proximity sensor or control base. The difference in potential (or range of
difference in potential) necessary to operate the unit.
Switching Frequency-the actual number
of targets to which the sensor can respond in a given time period, usually
expressed as Hertz (cycles per second).
[Top of page]
Target-the part or piece being detected.
Terminal Base Linearity-T.B.L.
(End Point Linearity) - a method of defining linearity. The maximum deviation
of any data point on a sensor output curve from a straight line drawn between
the end data points on that output curve. (T.B.L. is approximately twice
the magnitude of B.F.S.L.).
Terminal Line-a theoretical slope for which
the theoretical end points are normalized at 0 and 100% of both measurand
and output. Interchangeability error is referenced to this line.
Temperature Error-the maximum change
in output, at any input pressure within the specified range, resulting from
a change in temperature.
Thermal Drift Chart-a chart illustrating
sensor operating variance due to changes in temperature.
Thick-Film-technology using silk screened
pastes to form conductor, resistor, themistors, and insulator patterns; screened
onto the substrate (usually ceramic) and cured by firing at elevated
temperatures.
Thin Film-a technology using vacuum deposition
of conductors and dielectric materials onto a substrate (frequently silicon)
to form an electrical circuit.
Threshold Response-a control type
that responds to the change in input signal level. Plug-in amplifiers are
either threshold or transition responsive.
Throw-the number of circuits that each individual
pole of a switch can control. The number of throws is completely independent
of the number of poles and number of breaks. A single-pole double-throw
single-break switch connects the common terminal of the switch to the normally
closed terminal when the plunger is free, but connects the common terminal
to the normally open terminal when the plunger is depressed. A single-pole
single-throw single-break switch has a common terminal and either a normally
open terminal or a normally closed terminal but not both.
Thru Scan-a scanning technique in which the
emitter (light source) is aimed directly at the receiver. Also called direct
scan and transmitted scan, since light is transmitted directly, not reflected
to the sensor. Presently, it is the only scanning technique commonly used
to scan distances greater than 40 feet.
Time Delay Before
Availability-also know as False Pulse Protection. Outputs are turned
Off when power is first applied during this time period.
Total Travel-the distance from the plunger
free position to the full overtravel point.
Transducer-a fully packaged, signal conditioned,
compensated and calibrated sensor.
Transfer, Contact
Material-see
Migration.
Transient Protection-circuitry to
guard against spikes induced on the supply lines by inductive sources such
as heavy motors or solenoids turning On and Off.
Transients-in electronic usage, usually refers
to an unwanted, temporary, large increase or decrease in a current or supply
voltage that only occurs occasionally. Almost always due to reactive components
during rapid changes in voltage or current.
Transition Responsive-a control
type that responds to the rate of change in light intensity rather than the
level change. Used to detect fast moving objects that cause little change
in light intensity level.
Translucent-allows light to pass through.
Detecting translucent objects is often best done with retroreflective scan,
during which the light must pass through the object twice, thereby causing
more of a signal change (larger signal ratio).
Transmitter-a transducer with a current
loop output, typically 4 to 20 mA, enabling transmission of a signal over
a longer distance.
TTL-a generic term for Transistor Logic which is
used extensively in digital electronics systems.
TTL Compatibility-TTL
(transistor-transistor-logic) requires NPN (current sinking) input signals.
Reliable operation demands maximum input sensor voltage drop of 0.8 V. Most
TTL compatible interface devices have voltage drops of less than 0.7V.
Typical-(as used herein): refers to the target
value or where a range is given, represents an estimate of where 2/3 of the
total population of several production runs would be.
[Top of page]
UL-Underwriter's Laboratories, Inc., a non-profit
organization that establishes, maintains and operates laboratories for the
examination and testing of devices, systems and materials primarily for safety.
Unidirectional Differential Pressure
Sensor-a differential pressure sensor requiring the greater input
pressure to be applied to a specified pressure port.
Unshielded Sensor-a sensor with limited
side and front sensing capabilities.
Usable Sensing Distance-sensing
distance after temperature range tolerance and manufacturers tolerance are
taken into account.
[Top of page]
Velocity-the rate at which the position of
a moving object is changing. Velocity has two characteristics: magnitude
(speed) and direction.
Voltage-units = Volts (DC) or Volts RMS (AC).
The term used to designate the electrical energy, differential that exists
between two points and is capable of producing the flow of current when a
closed path is connected between the two points.
Voltage Drop-units = Volts (DC) or Volts
RMS (AC). Sometimes referred to as Saturation Voltage. In any solid state
control that switches a load, there will be some voltage dropped across the
output. This voltage drop or saturation voltage will often vary with the
amount of current going through the output section and the load. It should
be specified with current conditions.
[Top of page]
Welding, Contact-one of several conditions
that may cause switch contacts to fail to separate at the intended point
of plunger travel. As the name implies, the contacts literally are welded
together as a result of the electrical and thermal effects at the contact
interface.
[Top of page]
[Top of page]
[Top of page]
[Top of page]
|