Honeywell Logo

Sensing and Control

Conclusion

The soon to be announced DOE standards for 1999 will certainly change the design of appliances for the future. This new generation of appliances promises to bring new challenges to the designers but also new levels of performance, economy, and environmental friendliness to the purchasing consumer.

The application of electronics, sensors and control technology to appliances will enable the machines to achieve even better washability performance while providing better energy efficiency. OEM's using this strategy should be able to easily meet the new standards and avoid the high cost of designing new appliances.

Figure 6. Building blocks for smart appliances

Turbidity sensing will be one of the key technologies used to meet the performance standards for the late 90's. When combined with advanced algorithms, this technology can provide the information for the controller to see what is taking place during the wash process and to adapt itself intelligently to the task at hand.

Smart appliances like these can avoid washing dishes more (or less) than they need to be. They save water where they can by working to eliminate extra fills. They give more consistent results by moving the cycle selection away from the user, who typically uses the pots and pans cycle for every load, and do a better job interpreting true load conditions. They can feed information back to the user. They offer the ability to incorporate diagnostics into the machine and reduce field service calls for the OEM. For the appliance designer developing wet appliances, turbidity sensing can be a valuable tool. It may be the key to solving your efficiency improvement needs.

Back.....Forward

   Terms & Conditions | Privacy Statement Webmaster