Honeywell Logo

Sensing and Control

Smart Wash Process Sensor

At the heart of Maytag’s new dishwasher is the Wash Process Sensor (WPS), a sensor subassembly that integrates four sensor functions to continuously monitor turbidity, conductivity, temperature, and lower wash arm rotation. The stream of information provided by the sensor is processed by the fuzzy logic controller and is used to guide the operation of the dishwasher. What the sensor does, in essence, is provide enough sensory data to the machine so that dishes can be effectively washed using a minimum of water and energy.

In the past, the control variable for a load of dirty dishes was time: Energy and water were wasted because appliances depended on fixed time-based cycles to clean dishes, regardless of how soiled the dishes were or the type or amount of detergent used. The idea behind a dishwasher equipped with sensors and fuzzy logic control is that water and energy resources can be conserved by continuously sensing load conditions and adapting machine cycles according to need.

Back ..... Forward
   Terms & Conditions | Privacy Statement Webmaster