Honeywell Logo

Sensing and Control

Temperature and Wash Arm Sensors

Completing the suite of sensors in the WPS are a thermistor for measuring temperature and a magnetoresistive sensor to monitor wash arm rotation. Both are conventional technology. Temperature is critical in determining the effectiveness of the detergent cleansing and the state of dryness. The wash arm sensor is used to monitor the rotation of the water-pressure-powered lower spray arm in the dishwasher. It employs a magnetically-sensitive device manufactured by Micro Switch to sense the passage of a magnet attached to the spray arm assembly. The processor in the WPS monitors this device to calculate wash arm rpm. The controller combines the wash arm sensor signal with observations from the current sensor monitoring the motor current to provide diagnostic feedback to detect if the wash arm is blocked. If the wash arm is obstructed, the dishwasher can alert the user.

Other external sensory inputs that help the fuzzy controller determine optimal cycle times and settings include monitoring the time between loads so the appliance can adjust for dried-on food, and counting the number of times the dishwasher door is opened to estimate the number of dishes.

Back ..... Forward
   Terms & Conditions | Privacy Statement Webmaster