|
Sensing and Control |
Turbidity Sensors |
Turbidity sensors can be described by three basic types: transmissive,
scattering, and ratio. Each of the three configurations has its own advantages
and disadvantages. For the design engineer, each represents a different option
depending on the type and levels of turbidity to be measured. Each type also
has unique output characteristics.
The different configurations increase in cost as the number and performance of required components both electrical and mechanical are increased. The selection of a sensor type should therefore be based on the acceptable cost for a given application and the level of performance required to achieve the desired results. All of these sensor types typically use visible light for a source, and therefore they must be shielded from stray or ambient light. Low cost LED's are often used as a light source because they offer a trade-off between cost and convenience versus performance. Infrared sources have also been used. Incandescent light sources are sometimes preferable because they omit different wavelengths from the source. This helps to reduce the sensitivity of the turbidity sensor to variations in particle size. |
Transmissive sensorThe transmissive sensor configuration is low in cost, requiring only a light source and a detector. This sensor is usually placed so that it looks through the sides of a transparent tube through which the media under analysis flows. A example of the basic configuration is shown in Figure 3. While fairly easy to deploy, there are several critical design factors which can contribute to errors in the sensor output:
The characteristic output of this configuration is a signal which decreases monotonically with increasing turbidity. This type of sensor has been used on several Japanese clothes washers as a rinse detector to determine if additional rinsing is necessary for a particular load. Figure 3. Basic transmissive sensor configuration
|
|
|
Scattering sensorScattering sensors are also low in cost because they only require a light source and a detector. The scattering sensor differs from the transmissive sensor in that the alignment of the components is less critical. Various angles can be used to locate the detector depending on the desired sensitivity. Like the transmissive sensor, this sensor may be used to look through the sides of a transparent tube carrying the media under analysis, or it may be configured to look through the bottom of a vessel containing the media. Figure 4 illustrates a flow-tube application. Here too, several factors are critical to the sensor design:
The characteristic output of this sensor is an increased signal for increased turbidity which demonstrates high sensitivity to low turbidity conditions. Geometry is important because as the turbidity of the media increases, a point can be reached where the scattering phenomenon is overcome by the absorption of the media. This event causes foldback in the output. Figure 4. Basic scattering sensor operation
|
|
| Terms & Conditions | Privacy Statement | Webmaster |