Honeywell Sensing and Control is one of the world's largest single source suppliers
of sensors and switches.
Advantage
Page for:
- Product Manuals
- Product Drawings
- Configurators
- Software
- Latest Catalog
- And More
|
|
HONEYWELL INTRODUCES NEW UNIVERSAL PRESSURE
TRANSDUCER/TRANSMITER
Ruggedness and accuracy combined for Industrial
Sensing applications
COLUMBUS, OH., May 26, 2004 - Honeywell [NYSE: HON]
Sensing and Control announces a new universal pressure transducer/transmitter
from its Sensotec Test and Measurement business. The Model BDR sensor
delivers accuracies of +/-0.5% BFSL or +/-0.25% BFSL in the toughest
industrial applications, including hydraulic jackstands strong enough
to lift the Superdome, transmission testing and water-inventory
management. Constructed from all-welded stainless steel instead
of plastic, and available in ranges from 0-150 psi (10 bar) through
0-15,000 psi (1,500 bar), the Model BDR features configurable electrical
connections that maximize adaptability to varied applications. Thermal
error is low: +/-0.01% F.S./°C.
Versatility is key to the Model BDR's usefulness. Unlike many
similar sensors it is not industry dependent, and can handle essentially
any process gas or fluid and serve as a drop-in OEM replacement
for older sensors. According to designer Brian Richards, the Model
BDR is " an entry-level product with much higher specs than
you'd usually find in this type of sensor."
For more information visit www.honeywell.com/sensotec
or e-mail sales@sensotec.com.
|
| Honeywell International is a $23 billion diversified technology
and manufacturing leader, serving customers worldwide with aerospace
products and services; control technologies for buildings, homes
and industry; automotive products; turbochargers; specialty chemicals;
fibers; and electronic and advanced materials. Based in Morris Township,
N.J., Honeywell’s shares are traded on the New York, London,
Chicago and Pacific Stock Exchanges. It is one of the 30 stocks
that make up the Dow Jones Industrial Average and is also a component
of the Standard & Poor's 500 Index. For additional information,
please visit www.honeywell.com.
Honeywell Sensing and Control is part of Honeywell's Automation
and Control Solutions group, a global leader in providing product
and service solutions that improve efficiency and profitability,
support regulatory compliance, and maintain safe, comfortable environments
in homes, buildings and industry. For more information about Sensing
and Control, access www.honeywell.com/sensing.
| This release contains forward-looking
statements as defined in Section 21E of the Securities Exchange
Act of 1934, including statements about future business operations,
financial performance and market conditions. Such forward-looking
statements involve risks and uncertainties inherent in business
forecasts as further described in our filings under the Securities
Exchange Act. |
More Information
Other Announcements |
|