|
How can we be more efficient? One often overlooked area
is the rotating systems used in manufacturing and power
generation. By examining torque on these systems, downtime
can be reduced, product quality improved and energy efficiency
maximized.
What is torque?
It's a measure of the forces that cause an object to rotate.
Reaction torque is the force acting on the object that's
not free to rotate. An example is a screwdriver applying
torque to a rusted screw.
With rotational torque, the object is free to rotate.
Examples include industrial motor drives and gear reducers.
Torque and RPM determine horsepower, and horsepower determines
system efficiencies.
Torque measurements are used for process control. For example,
a lumber mill uses a predetermined maximum torque to initiate
blade changes. This saves wear and tear on the drive system
and increases product quality.
Many similar applications exist in manufacturing. Monitoring
torque is sometimes critical to the performance of axles,
drive trains, gear drives, and electric and hydraulic motors.
Other in-plant applications include gas and steam turbines.
|
|
Figure 1:
Moment arm, rotary transformer and slip ring methods
for measuring shaft torque |
Figure 2:
Wireless torque monitoring systems, including clamp-on
colla strained-gaged shaft and inline torque cell |
Getting the measurements
The need for torque measurements has led to several methods
of acquiring reliable data from objects moving. A torque
sensor, or transducer, converts torque into an electrical
signal.
The most common transducer is a strain gage that converts
torque into a change in electrical resistance. The strain
gage is bonded to a beam or structural member that deforms
when a torque or force is applied. Deflection induces a
stress that changes its resistance. A Wheatstone bridge
converts the resistance change into a calibrated output
signal.
The design of a reaction torque cell seeks to eliminate
side loading (bending) and axial loading, and is sensitive
only to torque loading.
The sensor's output is a function of force and distance,
and is usually expressed in inch-pounds, foot-pounds or
Newton-meters.
Reaction torque sensors are used when limited rotation
won't damage the cable. Its use minimizes the error attributable
to the inertia of rotating components. They are used to
calibrate torque wrenches, test the breaking torque of aircraft
fasteners and monitor the opening torque of child-proof
containers.
Other widely accepted methods for measuring torque rely
on mounting transducers in the machine train or on the rotating
shaft. With few exceptions, these methods use strain gages.
Each method has advantages and limitations, many of which
are application dependent. The best solution requires an
in-depth understanding of the application.
Two common ways to obtain torque measurements are by strain-gaging
the shaft and by using in-line torque cells. Both have two
technical obstacles: getting power to the gages over the
stationary/rotating gap and getting the signal back. The
methods to bridge the gap are either contact or non-contact.
Gaging the shaft
With strain gages bonded to the shaft, the shaft becomes
the transducer.
The general guideline is that the applied torque must
induce at least 150 to 175 micro-strain. The second requirement
is for the shaft to be calibrated, a process that usually
involves loading the shaft statically and tabulating the
results. This is relatively easy to do in small systems,
but as loads and shaft size increase, it becomes an onerous
task. Selecting a location for the strain gages, mounting
them carefully and protecting them become problematic for
users inexperienced in such techniques. Outside contractors
are usually available through the torque sensor suppliers
for most applications and locations.
Constant movement
Slip rings are used in contact-type torque sensors to apply
power to and retrieve the signal from strain gages mounted
on the rotating shaft. Slip rings are susceptible to wear.
Maintaining an oil-free slip ring is not always easy in
many industrial applications. Slip ring brushes, as well
as the support bearings internal to these torque sensors,
eventually wear out.
Figure 1 shows three common hardwired measurement schemes.
Non-contact methods
Radio telemetry of the signal coupled with wireless induced
power for the strain gage excitation offers an easy solution
for bridging the stationary-rotating gap. A stationary antenna
induces power in a loop antenna on the rotating shaft. The
power from the rotating shaft antenna is conditioned and
excites the strain gages. A shaft-mounted radio transmitter
sends the measurement signal back to the stationary antenna.
The telemetry antennas need to be somewhat flexible for
ease of mechanical installation, and receivers should have
adjustments for peak coupling of the antenna for maximum
induced power and received signal strength.
The radio antenna gap is normally less than 3/4 in. Radio
telemetry systems are reliable and easy to install, but
cost more. Their main advantage is the lack of contact and
need for maintenance. There are no support bearings or mechanical
contacting parts to wear out.
In-line rotary torque transformers are best for measuring
torque when transducers are mounted inline with the rotating
shaft. These consist of a strain gage torque cell having
a calibrated output and inductively coupled to the stationary
windings on the assembly by a rotary transformer.
The rotary transformer couples the strain gages for power
and signal return. The rotary transformer works on the same
principle as any conventional transformer except either
the primary or secondary coils rotate. The rotary transformer
is simple and easy to use, and is usually applied to smaller
machine trains. Rotary transformers have some susceptibility
to noise and require bearings for support, which also implies
maintenance. The act of mounting the in-line transducer
changes system dynamics and can mean the torque values themselves
may change.
Figure 2 shows typical wireless measurement schemes.
In-line wireless torque cells
Wireless torque cells consist of a rotary torque transformer
connected in-line with standard industry flanges, coupled
to the stationary portion of the assembly by wireless transmission.
It includes a stationary loop antenna that induces power
into an embedded antenna on the rotating torque cell, which
supplies the excitation voltage to the strain gages and
power to the radio transmitter mounted in the torque sensor.
The radio transmitter modulates the strain signal for transmission
to a stationary antenna. In-line torque cells offer high
torsional stiffness to maintain system dynamics.
They are pre-calibrated, and most have an internal calibration
system that supplies a calibrated output signal to adjust
instrument span in the absence of a known static torque.
The wireless telemetry feature eliminates support bearings
and their maintenance. In-line torque systems require cutting
the shaft or lengthening the machine train to accommodate
the inserted in-line transducer.
Clamp-on torque cells
A clamp-on torque cell works on the wireless telemetry
principle with the inherent advantages of a non-contact
system. It's immune to oil and dirt, but has the advantage
of not requiring the rotating shaft to be cut. The clamp-on
torque cell is a pre-calibrated bending beam mounted between
two collars that clamp on the shaft (see Figure 3). Accurately
spaced knife-edges provide an accurate, reliable shaft torque
measurement without marring or modifying the shaft. The
clamp-on feature allows the torque measuring system to be
moved to other similar installations easily in less than
30 minutes. This means the unit is ideal when torque or
horsepower monitoring forms part of the final check-out
of multiple machines. It handles shaft diameters from 3
to 32 in. and as much as 100,000 hp.
 |
Measuring torque on static
or rotating machinery is important for maintaining
quality and for continuous operation without downtime.
The direct torque sensor measurement is preferred
over the remote or indirect methods of calculating
torque.
Selecting a torque sensor for your application depends
upon the required long-term reliability, physical
constraints, portability and budget |
Figure
3. Clamp-on torque cell |
|