Test & Measurement

Site Map

Advantage Page for:

  • Product Manuals
  • Product Drawings
  • Configurators
  • Software
  • Latest Catalog
  • And More


Miniature load cells

Introduction
Sizes and Form Factors
Load Ranges
High Accuracy
Choosing the Right Load Cell
Rugged Construction
Immunity to Off Axis Loading
Fully Welded Assemblies
Detailed Model Information
Mounting Applications
Options
   Submersible Version
   Overload Stops
   Accessories

Options: Submersible Version

The submersible option is available on the model 31 and the model 53. This option adds a hermetic cable entry to the load cell using a glass to metal seal. It should be noted that the model 31 is resistant to the barometric effect of the fluid on the load cell.

The barometric effect is where the pressure of the liquid causes loading to be exerted on the load cell that is seen as a zero offset. This loading can be significant if the depth or pressure of the liquid is large or the capacity of the load cell is small. In these cases the zero offset will be a significant portion of full scale output.

figure 8

Fig 8 The barometric effect on submersed load cells

Back

Categories


View All:


Amplified High Output
Load Cells

Amplified High Output

Calibration Class
Load Cells

Calibration Class

Low Profile
Load Cells
Pancake Type
Fatigue Rated
Non-fatigue Rated

Miniature and Subminiature
Load Cells

Subminiature Size

Canister
Load Cells

Canister Type

In-Line
Load Cells

In-Line

Donut
Load Cells

Donut Shape

Beam
Load Cells

Beam Type

S-Beam
Load Cells

S-Beam Type

Special Application
Load Cells

Automotive Type

Accessories


Certificates | Privacy Statement | Search

1-800-867-3888   |  Request Information

Copyright 2004-2008 Honeywell International Inc. All rights reserved.