Test & Measurement

Site Map

Advantage Page for:

  • Product Manuals
  • Product Drawings
  • Configurators
  • Software
  • Latest Catalog
  • And More

VM VIBRATION METER FROM HONEYWELL SENSOTEC

COLUMBUS, OH., June 28, 2004—Honeywell [NYSE: HON] Sensing and Control announces a convenient hand-held vibration meter from its Sensotec Test and Measurement business. The portable, battery-powered Model VM from Honeywell Sensotec, Columbus, Ohio, enables engineers to prevent damage to components or bearings by monitoring machine vibration. Placing the probe directly on the vibration point and comparing two successive readings indicates when vibration is increasing to unacceptable levels. Users can select peak (VM110) or peak to peak (VM120) and rms measurements of acceleration, velocity, and displacement. Respective ranges for the three measurements are 2, 20, and 200 g; 2, 20, and 200"/sec; and 2 20, and 200 thou, respectively. Accuracies are 1.5% rms, 3% peak; 2.5% rms, 4% peak; and 3.5% rms, 5% peak, respectively. A low-pass filter selector removes signal noise. The LCD display provides 3 readings/s. (800-848-6564, fax 614-850-1111, www.honeywell.com/sensotec)

Honeywell International is a $23 billion diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; specialty chemicals; fibers; and electronic and advanced materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, Chicago and Pacific Stock Exchanges. It is one of the 30 stocks that make up the Dow Jones Industrial Average and is also a component of the Standard & Poor's 500 Index. For additional information, please visit www.honeywell.com. Honeywell Sensing and Control is part of Honeywell's Automation and Control Solutions group, a global leader in providing product and service solutions that improve efficiency and profitability, support regulatory compliance, and maintain safe, comfortable environments in homes, buildings and industry. For more information about Sensing and Control, access www.honeywell.com/sensing.

This release contains forward-looking statements as defined in Section 21E of the Securities Exchange Act of 1934, including statements about future business operations, financial performance and market conditions. Such forward-looking statements involve risks and uncertainties inherent in business forecasts as further described in our filings under the Securities Exchange Act.

 

More Information    Other Announcements

Certificates | Privacy Statement | Search

1-800-867-3888   |  Request Information

Copyright 2004-2008 Honeywell International Inc. All rights reserved.