Editorial contact: Royer
Slater
Honeywell Control Systems Ltd
Direct to desk: 01344 656379 |
Ref: UK98/00 |
British Gas’s “Aspect” magazine praises Honeywell Smartfit
as “a new de facto standard for the future of
central heating controls”
BRACKNELL, UK, 12 DECEMBER 2000 – Honeywell’s Smartfit central heating control system has been praised as “a new de facto standard for the future of central heating controls” in British Gas’s “Aspect” magazine, published for British Gas engineers.
“It is flattering that British Gas decided to commission a five page editorial dedicated to this revolutionary control system for heating and hot water control,” commented Mike Ward, Honeywell Home and Building Control Products Vice President.
“Aspect” magazine describes Smartfit as revolutionary because it “not only completely eliminates the need for traditional complex wiring but also provides a built-in diagnostic program that automatically indicates a system fault and highlights where the fault lies.”
The British Gas article places special emphasis on both the ease of installation and the innovations made for servicing. It explains that all the Smartfit control system’s components are connected using simple plug-in or two-wire connections, whilst a commissioning check built into the Smartfit’s intelligence ensures the system it is working correctly. “Should a system failure occur, either during commissioning or normal operation, an ‘F’ fault code (ranging from F1 to F15) will be displayed on the room unit’s LCD window,” the report says.
Said Mike Ward, “This article is an unmistakable acknowledgement of Honeywell’s innovation and recognition of Honeywell’s pledge to create products that respond to the requirements of ever more demanding customers.”
Honeywell Home & Building Control is a US$5.5 billion business that provides products and services to create efficient, safe, comfortable environments. The business offers controls for heating, ventilation, humidification and air-conditioning equipment, security and fire alarm systems, home automation systems, energy-efficient lighting controls and building management systems and services.
Honeywell is a US$24-billion diversified
technology and manufacturing leader, serving customers worldwide with aerospace products
and services; control technologies for buildings, homes and industry; automotive products;
power generation systems; specialty chemicals; fibres; plastics; and electronic and
advanced materials. The company is a leading provider of software and solutions, and
Internet e-hubs including MyPlant.com, MyFacilities.com and MyAircraft.com (joint venture
with United Technologies and i2 Technologies). Honeywell employs approximately 120,000
people in 95 countries and is traded on the New York Stock Exchange under the symbol HON,
as well as on the London, Chicago and Pacific stock exchanges. It is one of the 30 stocks
that make up the Dow Jones Industrial Average and is also a component of the Standard
& Poors 500 Index. Additional information on the company is available on the
Internet at www.honeywell.com.
This release contains forward-looking
statements as defined in Section 21E of the Securities Exchange Act of 1934, including
statements about future business operations, financial performance and market conditions.
Such forward-looking statements involve risks and uncertainties inherent in business
forecasts.
# # #
Honeywell Control Systems
Ltd
Honeywell House, Arlington Business Park
Bracknell, Berkshire RG12 1EB
01344 656000. Fax: 01344 656240.
Enquiries e-mail: uk.infocentre@honeywell.com
Web: www.honeywell.com/uk
Editorial contact: Royer Slater
Honeywell Control Systems Ltd
Direct to desk: 01344 656379
royer.slater@honeywell.com |