Home>Worldwide Sites


SEARCH

SITE MAP

HONEYWELL IN THE NEWS

HONEYWELL IN THE UK

SOLUTIONS FOR:
- Homes

- Buildings

- Industry

- Aviation

-Sensing & Control

FORTHCOMING EVENTS

YEAR 2000


 

IN THE NEWS
 
Editorial Contact: Royer Slater
Honeywell Control Systems Ltd
Switchboard: 01344 656000

royer.slater@honeywell.com Ref: UK 42/01

The Domestic Heating and Plumbing Trade Events: Honeywell provides valuable advice, answers technical questions and demonstrates the latest heating control technologies. 

BRACKNELL, 14 SEPTEMBER 2001    Honeywell, the leading supplier of controls to the domestic heating market, provides valuable advice on maximising the trade’s profitability, answers technical questions and demonstrates the latest heating control technologies to visitors at the regional Domestic Heating and Plumbing Trade Events (DHPTE) this autumn.
“We are there to answer installers’ problems, rather than just to show the latest products,” said Richard Edwards, Manager of Honeywell’s Trade Business.

Key among the Honeywell exhibits is the Smartfit system, now established as a new standard for central heating control – not surprising as it was developed in response to installers demands for a system that is not only quick and easy to install but includes self-diagnostics to show if there is a fault.  It helps specifiers, merchants and installers by reducing the complexity of installation and ensures the installation is “right first time”.  Its connections are either plug in or have two wire connections that are polarity free, resulting in reduced hassle and inconvenience.  If there is a central heating problem in the future, the householder can pass on a fault code from the Smartfit controller’s display, identifying the problem and allowing the correct parts to be taken to fix it.

Traditional control solutions are still of major importance, so Honeywell is demonstrating products to develop this market, including reversible flow radiator thermostats and advanced controls such as the CM60 programmable room thermostat range. With the growth of combi boiler installations, Honeywell offers both wired and wireless (RF) control solutions.

Honeywell is committed to expanding the market, so it holds regular training courses around the country to help installers keep up to date with the latest technologies.  Honeywell is also involved in lobbying the Government to raise the standard of energy efficiency controls in the UK.

All Honeywell products comply with UK and European directives and are manufactured in factories certificated to ISO 9000.  Established in 1885, Honeywell have a reputation for high quality products that meet every control requirement in all its business areas including applications as diverse as aerospace, industrial processes and commercial buildings.

Dates and venues for DHPTE shows this autumn are:

Cardiff Millennium Stadium    13th September
Brands Hatch, Kent  26th September
Plymouth Moat House Hotel     18th October
Silverstone Motor Racing Circuit, Northants      24th October
Wolverhampton Wanderers Football Club    21st November
Norwich City Football Club 27th November

Readers can request further details of the Honeywell Smartfit system from: 
Honeywell Control Systems Ltd., Honeywell House, Arlington Business Park, Bracknell, Berkshire RG12 1EB.  
Freephone: 0800 521121.  
Switchboard: 01344 656000. 
Fax: 01344 656240. 
Email: uk.infocentre@honeywell.com
Web: www.honeywell.com/uk

Honeywell is a US$25-billion diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; power generation systems; speciality chemicals; fibres; plastics; and electronic and advanced materials.  Honeywell employs approximately 120,000 people in 95 countries and is traded on the New York Stock Exchange under the symbol HON, as well as on the London, Chicago and Pacific stock exchanges.  It is one of the 30 stocks that make up the Dow Jones Industrial Average and is also a component of the Standard & Poor’s 500 Index.  Additional information on the company is available on the Internet at www.honeywell.com.

This release contains forward-looking statements as defined in Section 21E of the Securities Exchange Act of 1934, including statements about future business operations, financial performance and market conditions.  Such forward-looking statements involve risks and uncertainties inherent in business forecasts as further described in our filings under the Securities Exchange Act

# # #

 

 

Honeywell Control Systems Ltd
Honeywell House, Arlington Business Park
Bracknell, Berkshire RG12 1EB
Tel: 01344 656000. Fax: 01344 656240.
Enquiries e-mail: uk.infocentre@honeywell.com
Web :
www.honeywell.com/uk




Copyright © 1999 Honeywell. All rights reserved