Home>Worldwide Sites


SEARCH

SITE MAP

HONEYWELL IN THE NEWS

HONEYWELL IN THE UK

SOLUTIONS FOR:
- Homes

- Buildings

- Industry

- Aviation

-Sensing & Control

FORTHCOMING EVENTS

YEAR 2000


 

IN THE NEWS
 
Editorial contact: Royer Slater
Honeywell Control Systems Ltd
Direct to desk: 01344 656379
Ref: UK11/01A

Honeywell's Temaline: a new concept in access control, time and attendance recording, intruder detection and integrated security and security communications

BRACKNELL, UK, 21 MARCH 2001 - Honeywell's EBI Temaline products and architecture provide a new system for integrated access control, time and attendance recording, and intruder detection for customers in Europe, Middle East and Africa. EBI Temaline brings enhanced performance and reliability to security installations through peripheral controllers called TemaServers and a wide-range of LON-based field-mounted user devices, TemaKeys, which include a variety of card readers, pinpads, keyboards, digital I/O devices and user terminals. With EBI Temaline, users benefit from the highest levels of system availability and reliability - a solution that is dependable and scaleable, which meets the exact needs of their facilities today and is readily expandable for future growth.

EBI Temaline manages access control, intruder detection and time and attendance using a systems architecture, which matches users' IT standards. Native Ethernet communications protocols allow real-time event management and direct peer-to-peer communication across an Ethernet backbone and a LonWorksä-compatible field-bus network.

TemaServers and TemaKeys are an integral component of Honeywell's Open Enterprise Buildings Integrator (EBI) environment, which provides seamless interoperability and "single window" operator access to a variety of Building Automation subsystems. This "integration by design" provides benefits that reach across the automation application spectrum to include integrated security applications - such as Access Management, Intruder Detection, Digital Video Management and Photo ID - HVAC (heating ventilating and air conditioning), Safety Management Solutions such as Fire Detection and Audio Evacuation, as well as Personnel and Payroll management with Time and Attendance recording.
A Honeywell survey of customers identified system availability and reliability as their primary concerns. A failure of the supervisory system or loss of communications can cause serious problems to a user's facility operations. In developing the EBI Temaline system, Honeywell has three-way redundancy capability, up to now never achieved by any Security solution. Firstly independent modularity frees the peripheral and field devices from reliance on the central supervisory system for all access control operations, thus relieving the supervisory system of card transaction processing. Secondly, Honeywell's unique "Shared Load" concept virtually guarantees continuity of the system. Should a TemaServer fail, another takes over management of its field device TemaKeys without degrading the performance of the EBI Temaline system. Finally, a removable Flash EPROM cartridge in each TemaServer further guarantees complete data recovery of employee card transactions in the unlikely event that all management systems should fail.

As an open environment, EBI allows users to use their own company database to manage cardholder information and share this with Enterprise Resource Planning systems such as SAP, Oracle and PeopleSoft to address the broadest of Enterprise management requirements.
Readers can request further details from: Honeywell Home and Building Control, Honeywell House, Arlington Business Park, Bracknell, Berkshire
RG12 1EB. Tel: 01344 656000. Fax: 01344 656240.
E-mail: uk.infocentre@honeywell.com Web: www.myserviceandsolutions.co.uk 

Honeywell Home & Building Control is a US$5 billion business that provides products and services to create efficient, safe, comfortable environments. The business offers controls for heating, ventilation, humidification and air-conditioning equipment, security and fire alarm systems, home automation systems, energy-efficient lighting controls and building management systems and services.

Honeywell is a US$25-billion diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; power generation systems; specialty chemicals; fibres; plastics; and electronic and advanced materials. The company is a leading provider of software and solutions, and Internet e-hubs including MyPlant.com, MyFacilities.com and MyAircraft.com (joint venture with United Technologies and i2 Technologies). Honeywell employs approximately 120,000 people in 95 countries and is traded on the New York Stock Exchange under the symbol HON, as well as on the London, Chicago and Pacific stock exchanges. It is one of the 30 stocks that make up the Dow Jones Industrial Average and is also a component of the Standard & Poor’s 500 Index. Additional information on the company is available on the Internet at www.honeywell.com.

This release contains forward-looking statements as defined in Section 21E of the Securities Exchange Act of 1934, including statements about future business operations, financial performance and market conditions. Such forward-looking statements involve risks and uncertainties inherent in business forecasts.

# # #

Honeywell Control Systems Ltd
Honeywell House, Arlington Business Park
Bracknell, Berkshire RG12 1EB
01344 656000. Fax: 01344 656240.
Enquiries e-mail: uk.infocentre@honeywell.com
Web: www.honeywell.com/uk

Editorial contact: Royer Slater
Honeywell Control Systems Ltd
Direct to desk: 01344 656379
royer.slater@honeywell.com




Copyright © 1999 Honeywell. All rights reserved