|
Honeywell warns over - 65's and their carers of
scalding danger in the bathroom.
Honeywell lists recommendations to prevent
scalding among the elderly.
BRACKNELL,
UK, 3 SEPTEMBER 2002 -
The elderly are at particular risk of life threatening
scald burns, warns Honeywell, the leading controls company.
These dangers to over-65s occur most commonly in the
bathroom and are much less widely promoted than for toddlers under
two – the other high risk group.
“While
both age groups are particularly prone to scald burns due to their
thinner skin, the elderly
are at increased risk because their skin tends to be less
sensitive, so they might not be able to
pull away from hot water quickly enough to avoid scalding,”
notes Matthew Gordon of Honeywell.
“They also tend to be less agile and so are at risk of
injury while trying to escape from a scalding bath or a blast of
hot water from a shower. Scalding
injuries often cover a large area of the body, leading to high
rates of morbidity and mortality.
People
who are physically or mentally impaired are particularly at risk
due to their slower reaction times and inability to respond.
Within
care homes, to prevent risks from Legionella, hot water must be
stored and distributed at high temperatures.
So there must be fail-safe mixing control at the outlet to
prevent scalding, states Honeywell, whose tamperproof thermostatic
mixing valves ensure water to baths and showers is delivered at a
pre-set safe temperature. The
same risks are present for these people in their own homes as well.
This
is specified in Standard 25 of the UK Department of Health’s
National Minimum Standards for Care Homes for Older People,
published by the Secretary of State for Health under Section 23(1)
of the Care Standards Act 2000, as follows: “Water is stored at
a temperature of at least 60 degrees C and distributed at 50
degrees minimum, to prevent risks from Legionella. To prevent risks from scalding, pre-set valves of a type
unaffected by changes in water pressure and which have fail safe
devices are fitted locally to provide water close to 43 degrees
C.”
The
standard is applicable to care homes which provide accommodation
together with nursing or personal care.
Honeywell gives the following advice to elderly people
living in the community and to their carers:
-
Always
use the “elbow test” to check bath water temperature
before bathing. The
water should be warm, not hot.
Or use a thermometer – over 43 degrees C is too hot.
-
Consider
installing a thermostatic mixing valve, which ensures the
water in the bath is at a safe temperature.
-
Never
leave a full bath unattended, the vulnerable person may climb
unwittingly into scalding water and be unable to get out.
-
Be
vigilant whenever a handicapped person under your care takes a
bath. Ensure they do not turn on the hot water tap if the hot
water is at the usual storage temperature – 60 degrees C or
above – as it will scald them.
-
Always
run cold water into a bath
first.
If
someone gets burnt or scalded, Honeywell reminds carers that the
government advises them to:
-
Keep
the affected area under cold water for as long as possible (at
least 10 minutes).
-
Don't
remove anything sticking to the injury. Cover it with sterile,
non fluffy material; cling - film is ideal.
-
Do
not apply anything to the scald (for example, no creams,
ointment, fat or ice).
-
For
any size of burn, you should seek immediate medical attention.
Honeywell’s
TM200V thermostatic mixing valve mixes the hot and cold supply to
deliver water at a pre-set temperature.
A lockable safety cap displays the temperature set point
and prevents tampering. It
is ideal for nursing homes, hospitals, sheltered housing and
playgroups. Two sizes
are available, 15mm and 22mm, making it suitable for baths,
basins, bidets and showers.
Honeywell
is a US$24-billion diversified technology and manufacturing
leader, serving customers worldwide with aerospace products and
services; control technologies for buildings, homes and industry;
automotive products; power generation systems; speciality
chemicals; fibres; plastics; and electronic and advanced
materials. Honeywell employs approximately 115,000 people in 95
countries and is traded on the New York Stock Exchange under the
symbol HON, as well as on the London, Chicago and Pacific stock
exchanges. It is one of the 30 stocks that make up the Dow Jones
Industrial Average and is also a component of the Standard &
Poor’s 500 Index. Additional
information on the company is available on the Internet at
www.honeywell.com.
This
release contains forward-looking statements as defined in Section
21E of the Securities Exchange Act of 1934, including statements
about future business operations, financial performance and market
conditions.
Such forward-looking statements involve risks and
uncertainties inherent in business forecasts as further described
in our filings under the Securities Exchange Act
# # #
Honeywell Control Systems
Ltd
Honeywell House, Arlington Business Park
Bracknell, Berkshire RG12 1EB
01344 656000. Fax: 01344 656240.
Enquiries e-mail: uk.infocentre@honeywell.com
Web: www.honeywell.com/uk
|