Editorial contact: Royer
Slater
Honeywell Control Systems Ltd
Direct to desk: 01344 656379 |
Ref: UK99/00 |
Built to last: Honeywell introduces new corrosion-resistant pressure reducing valve
Minimises water consumption and repair costs by protecting
installations against damage from excessive pressure
in the water supply.
BRACKNELL, UK, 22 DECEMBER 2000 – Honeywell’s corrosion-resistant D15P pressure reducing valve now features an epoxy powder coating that protects valve components, so ensuring long-term, reliable operation in underground chambers. The epoxy powder coating is applied inside and outside the valve body to provide a high degree of protection against corrosion. The powder coating is physiologically safe and non-toxic.Other new features include an increased outlet pressure range of 1.5 to 8.0 bar and a position indicator on the spring bonnet to provide easier setting.
Built to a reliable and well-proven design, the Honeywell D15P is designed for use in potable water supply systems and is used in municipal, industrial and commercial water networks. It is WRc approved for use with potable water and all materials in contact with the water are KTW approved. It also carries full WRAS approval.
Honeywell D15P pressure reducing valves minimise water consumption and repair costs by protecting water installations against damage from excessive pressure in the water supply. By reducing the operating pressure and maintaining it at a constant level, the Honeywell D15P also minimises flow noise in the installation. They can be used in multi-dwelling buildings as well as industrial and commercial premises. The set output pressure is held constant across a wide inlet pressure fluctuation.
Honeywell supplies the D15P in sizes from 50mm to 200mm (DN 50 to DN 200) and with a maximum inlet pressure rating of 16.0 bar.
Readers can request further details from: Honeywell Control Systems Ltd., Honeywell House, Arlington Business Park, Bracknell, Berkshire RG12 1EB. Tel: 01344 656000. Fax: 01344 656240. E-mail:
uk.infocentre@honeywell.com
Web: www.honeywell.com/uk
Honeywell Home & Building Control is a US$5.5 billion business that provides products and services to create efficient, safe, comfortable environments. The business offers controls for heating, ventilation, humidification and air-conditioning equipment, security and fire alarm systems, home automation systems, energy-efficient lighting controls and building management systems and services.
Honeywell is a US$24-billion diversified
technology and manufacturing leader, serving customers worldwide with aerospace products
and services; control technologies for buildings, homes and industry; automotive products;
power generation systems; specialty chemicals; fibres; plastics; and electronic and
advanced materials. The company is a leading provider of software and solutions, and
Internet e-hubs including MyPlant.com, MyFacilities.com and MyAircraft.com (joint venture
with United Technologies and i2 Technologies). Honeywell employs approximately 120,000
people in 95 countries and is traded on the New York Stock Exchange under the symbol HON,
as well as on the London, Chicago and Pacific stock exchanges. It is one of the 30 stocks
that make up the Dow Jones Industrial Average and is also a component of the Standard
& Poors 500 Index. Additional information on the company is available on the
Internet at www.honeywell.com.
This release contains forward-looking
statements as defined in Section 21E of the Securities Exchange Act of 1934, including
statements about future business operations, financial performance and market conditions.
Such forward-looking statements involve risks and uncertainties inherent in business
forecasts.
# # #
Honeywell Control Systems
Ltd
Honeywell House, Arlington Business Park
Bracknell, Berkshire RG12 1EB
01344 656000. Fax: 01344 656240.
Enquiries e-mail: uk.infocentre@honeywell.com
Web: www.honeywell.com/uk