|
Hometronic
system controls under floor heating, appliances and lightening
throughout the home, making it more comfortable and secure
Homeowners
can set up several profiles that match their lifestyle
–
telling Hometronic what to do, how and when.
BRACKNELL, UK,
25
FEBRUARY 2002 - Honeywell has introduced the latest version of its
advanced Hometronic wireless domestic automation system, which
makes a home more comfortable and secure, while reducing energy
consumption. The
Hometronic system uses RF (radio frequency) links to control a
home’s underfloor heating, lighting and appliances
automatically.
Homeowners can set up several profiles that match their
lifestyle. These tell Hometronic what to do, how and when.
Each profile can provide individual temperature control in
each room, as well as switching appliances, lights and services at
pre-programmed times or in response to certain events.
For example, it can close blinds and curtains when it gets
dark, or start a garden sprinkler when it is too dry.
A typical “wake up” profile might start laundry
machines during the night to take advantage of cheaper
electricity, raise temperatures in each room just before the
family wakes, then welcome them with fresh coffee from a coffee
maker that Hometronic has started automatically.
A single press of a button can take Hometronic into the
“Leaving” profile, which saves energy by reducing temperatures
throughout the home to lower values while the house is unoccupied,
then raises them again before the family’s homecoming.
If they arrive early, by pressing the “Arriving”
profile button the heating is started immediately.
An “evening” profile might adjust the temperatures in rooms to
different levels, to recognise that the family is at home, or that
different rooms are being used.
A “party” profile might postpone the time at which the
heating is reduced at night.
More importantly for the homeowner’s peace of mind, they can set
a “holiday” profile for use while the home is unoccupied.
This can create an impression of occupancy by switching
lights and opening and closing curtains, according to a normal
occupancy pattern. It
can reduce the heating to a level that minimises energy use but
prevents freezing. If
desired, it can detect a burst pipe and turn off the water supply,
shut off the gas if there’s a leak, or even water the plants in
the garden.
A single wall-mounted unit – the Hometronic Manager – allows
homeowners to override, change or switch between pre-programmed
profiles, or they can do so through an infra-red remote unit.
As
the Hometronic system is wireless, it is quick and easy to install
without damaging home decorations.
It uses a unique multi-frequency transmission radio
frequency (RF) system to ensure reliable and consistent operation.
Hometronic room modules
monitor the current temperature in each room and transmit by RF to
the Hometronic Manager, which can control up to 16 individual time
and temperature zones within the home using RF radiator
controllers. Other
Honeywell products, such as Air Conditioners and portable High
Efficiency Particle Air (HEPA) filter units, can be plugged into
any mains socket in the home, yet still be controlled by the
Hometronic Manager.
Readers can request further details of Honeywell Hometronic from
Honeywell Control Systems Ltd, Honeywell House, Arlington Business
Park, Bracknell, Berkshire RG12 1EB.
Tel: 01344 656000. Fax:
01344 656240.
E-mail: uk.infocentre@honeywell.com
Web:
www.honeywell.com/uk/homes.htm
Honeywell is a US$24-billion diversified
technology and manufacturing leader, serving customers worldwide with aerospace products
and services; control technologies for buildings, homes and industry; automotive products;
power generation systems; specialty chemicals; fibres; plastics; and electronic and
advanced materials. The company is a leading provider of software and solutions, and
Internet e-hubs including MyPlant.com, MyFacilities.com and MyAircraft.com (joint venture
with United Technologies and i2 Technologies). Honeywell employs approximately 120,000
people in 95 countries and is traded on the New York Stock Exchange under the symbol HON,
as well as on the London, Chicago and Pacific stock exchanges. It is one of the 30 stocks
that make up the Dow Jones Industrial Average and is also a component of the Standard
& Poors 500 Index. Additional information on the company is available on the
Internet at www.honeywell.com.
This release contains forward-looking
statements as defined in Section 21E of the Securities Exchange Act of 1934, including
statements about future business operations, financial performance and market conditions.
Such forward-looking statements involve risks and uncertainties inherent in business
forecasts.
# # #
Honeywell Control Systems
Ltd
Honeywell House, Arlington Business Park
Bracknell, Berkshire RG12 1EB
01344 656000. Fax: 01344 656240.
Enquiries e-mail: uk.infocentre@honeywell.com
Web: www.honeywell.com/uk
|