Contact: Royer Slater
Honeywell Control Systems Ltd
Direct to desk: 01344 656379royer.slater@honeywell.com
Ref: UK09/00
Honeywell Smartfit sets the new standard for central heating control
BRACKNELL, UK, 26 JANUARY 2000 - Honeywell, the most trusted name in central
heating controls, has launched a new system that removes the difficulty of wiring a home
central heating system and reduces installation time. Honeywell Smartfit features low
voltage wiring and plug-in control connections to minimise the chance of errors and to
make wiring quicker and simpler.
Honeywell introduced its Sundial Plans some thirty years ago and they were
quickly adopted as the industry standard. Honeywell now sets the new, de facto
standard for central heating controls with its low-voltage, plug-in Smartfit system.
Smartfit provides installers with greater productivity and the means to higher profit
margins.
"Smartfit marks the most fundamental change in the installation of home
heating controls since Sundial Plans," said Mike Ward, Honeywell UK Director of Home
and Building Control Products. "Few domestic appliances have not changed radically to
benefit from the latest technologies over the last thirty years. However, we recognise
that change is difficult in the domestic heating market, so Smartfit has been designed to
look and feel like a traditional system."
Central to Smartfit is a new connection box that provides plug-in or simple
2-wire connection for all space heating and hot water controls. There is no need for a
wiring diagram: installers simply connect the two-wire room unit, plug in the valves and
cylinder sensor, and the system is complete, whether it is an S-Plan or Y-Plan.
All Honeywell Smartfit system connections are low voltage and polarity-free.
Although installers still need to make mains voltage connections to the pump and boiler,
even these have been reduced to one wire per terminal. By comparison, traditional systems
require more than 30 wires to be prepared and connected correctly, mains voltage being
carried to every unit in the system and sometimes with several wires at a single terminal.
Honeywell Smartfit valves have snap-on actuator heads with plug-in connections
back to the base unit. The same actuator unit fits onto all valve bodies. The elegant
Smartfit programme controller provides a single point of control for all space heating and
hot water programmes. It also includes a built-in diagnostics facility that enables faults
to be quickly identified and remedied, reducing call-backs and saving installers
time and cost. The final component of the Honeywell Smartfit system is a cylinder sensor
that also features plug-in connections back to the base unit.
In developing Smartfit, Honeywell researched the biggest problems facing
installers and developed Smartfit to remove the difficulties of wiring and fault finding.
Honeywell also researched householders wishes, so that the Smartfit controller
brings together central heating and hot water control in a single, stylish unit.
All this, coupled with the established Honeywell renown for quality and
reliability, adds up to happy customers, profitable installation and enhanced reputation.
Readers can request further details from: Honeywell Control Systems Ltd.,
Honeywell House, Arlington Business Park, Bracknell, Berkshire RG12 1EB. Tel: 01344
656000. Fax: 01344 656240.
E-mail: uk.infocentre@honeywell.com
Web: www.honeywell.com/uk/homes/smartfit.htm
Honeywell is a US$24-billion diversified technology and manufacturing
leader, serving customers worldwide with aerospace products and services; control
technologies for buildings, homes and industry; automotive products; power generation
systems, speciality chemicals; fibres; plastics; and electronic and advanced materials.
The company employs approximately 120,000 people in 95 countries. Honeywell is traded on
the New York Stock Exchange under the ticker symbol HON, as well as on the London, Chicago
and Pacific stock exchanges. It is one of the 30 stocks that make up the Dow Jones
Industrial Average and is also a component of the Standard & Poors 500 Index.
Additional information on the company is available on the Internet at: http://www.honeywell.com
Note to editors: The merger involving AlliedSignal Inc. and Honeywell
Inc. became effective after close of trading on the New York Stock Exchange on December 1,
1999. In connection with the merger, AlliedSignal Inc. changed its name to Honeywell
International Inc. Its ticker symbol on the New York Stock Exchange was changed from ALD
to HON, which until closure had been Honeywell Inc.s ticker symbol.
Honeywell Europe, Middle East & Africa employs 25,500 people in 49
countries. Sales in 1999 were US$6.4-billion. The companys regional headquarters are
in Brussels.
# # #
Editorial contact:
Royer Slater (direct phone: 01344 656379; direct fax: 01344 656034)
Honeywell Control Systems Ltd
Honeywell House
Arlington Business Park
Bracknell
Berkshire RG12 1EB
Switchboard: 01344 656000. Fax: 01344 656240.
E-mail: Personal: royer.slater@honeywell.com
General: uk.infocentre@honeywell.com
Web: www.honeywell.com/uk
Notes to Editors
Text files: We will be pleased to provide our press releases as a
text file or as a document in most popular word processing packages, by e-mail or on disk.
Please contact us, as below.
Photos and illustrations: Honeywell can help publishers by
providing photos and illustrations "ready scanned" - eliminating the need for
colour separation processes and charges. The electronic files can be provided in all
recognised picture formats for you to insert directly into your publishing package, where
you may size and crop them as required. The files can be supplied by e-mail, on Iomega ZIP
disks or as 3.5" disks (for small file sizes). If you publish editorial pages by
stripping colour separations into four-colour film, we can provide a service for
four-colour separated film of our photos, to your requirements, usually within three
working days. Honeywells communications department in Bracknell will be pleased to
assist.
Honeywell supports the following joint initiatives of the
Chartered Institute of Journalists, Institute of Public Relations, National Union of
Journalists, Public Relations Consultants Association and Incorporated Society of British
Advertisers: