Honeywell UK Homepage           Home Controls Homepage

WHAT WE CAN OFFER


Application Guides

Building Regulations

Combustion Controls

Comfort Controls

End User

FAQ

Industry Links

Installer Training

Instllr./User Guides

Latest News

Literature

Product Families

Spare Parts

Technical Catalogue

Technical Support

Underfloor Heating

Water Products

Product Data


PROGRAMMABLE THERMOSTATS
 

Honeywell is the world leader in advanced heating technology. The introduction of the innovative CM60 series of programmable thermostats confirms our market leading position.

CM61 24hr Programmable Thermostat
CM67 7 day Programmable Thermostat
CM60RF Programmable Thermostat with RF
RTS Remote temperature sensor
OTS Outside temperature sensor
CM30 Programmable Thermostat - Analogue

CM61

The CM61 programmable thermostat has been designed to provide automatic temperature and time control of radiator, cooling and warm air heating systems. It may also be used for underfloor heating systems. The unit can directly switch circulating pumps and boilers, motorised zone valves and underfloor heating actuators. Voltage free contacts enable the CM61 to  control systems operating from 24 to 240v ac.

Intended for applications where the householder has the same heating needs from day to day, the CM61 features single function buttons to simplify programming and operation.

The optional optimum start model will delay the startup of the heating system to the latest possible moment, to avoid unnecessary energy use, so that the dwelling is comfortably warm by the programmed time.

CM67

The CM67 has all of the same functionality as the CM61, plus the capability of  providing a different heating programme for each day of the week.

CM61/67 RF  

Has been replaced by the new CM61/67 RF NG

The product pack will consist of a programmable thermostat and relay box. 

The user interface and programming of the CM60 RF NG is identical to the current model. 

Two packs will be available as detailed below: 

Y6667D1086 CM67 RF with optimum start – (replaces Y6667C1013 and Y6667C1021) 

Y6661D1074 CM61 RF with optimum start – (replaces Y6661C1019 and Y6661C1027) 

Both units are supplied with optimum start enabled. If this feature is not required, it may be disabled by the installer using the installer set-up mode. A label over the display describes this. 

Each system pack is pre-bound so no initial binding is required on site allowing quicker installations.

AUTOMATIC TIME SET MODULE

The optional Automatic Time Set Module (ATS) clips to the side of the Programmable Thermostat without the need for any additional wiring and checks the displayed time once per day by reference to the national time radio signal from the Rugby transmitter. The time is thus accurately maintained and changes automatically with the spring and autumn changes from GMT to BST.

REMOTE TEMPERATURE SENSOR

A hardwired room sensor allows the living space temperature to be sensed with the CM60 fited in a more suitable location: for example, where it is not easily accessibe to young children.

OUTSIDE TEMPERATURE SENSOR

A hardwired outsided sensor allows the householder to to display the outside temperature when required. (This does not provide outside temperature compensation)

CM30

Designed for the householder who wants the advanced features of digital technology but prefer the simplicity of analogue control settings, the CM30 series provides these options, all presented in the stylish Honeywell waveform design.

Available in both 24hr and 7 day versions, the CM30 series is the ideal programmable thermostat for any independent heating area, or for supplementary zones such as granny flats or attic conversion.

 

Honeywell’s Customer Information Centre in the UK has a new central e-mail address, uk.infocentre@honeywell.com which can be used to request details of Honeywell products and services for homes, buildings and industry.

PRIVACY STATEMENT

Copyright © 2005 Honeywell. All rights reserved
smallestlogo.gif (1482 bytes)

 

 

 

 

 

 

 

 

 

 

 

 

Cm6167.jpg (4061 bytes)
CM61/67

 

 

 

 

 


CM67RF

Read Overview
Installation
Manual
User Guide 24 hr
User Guide 7 day

 

 

 

 

 

ATS.JPG (1784 bytes)
ATS Module

 

 

 

 

 

 

 

 


CM30.JPG (346781 bytes)

 

CM30