Honeywell UK Homepage                             Home Controls Homepage

WHAT WE CAN OFFER


Application Guides

Building Regulations

Combustion Controls

Comfort Controls

End User

FAQ

Industry Links

Installer Training

Instllr./User Guides

Latest News

Literature

Product Families

Spare Parts

Technical Catalogue

Technical Support

Underfloor Heating

Water Products

Product Data


SPARE PARTS
 
Spare parts are an essential part of our portfolio of equipment supply and are offered for three distinct areas - Heating, Water and Gas.

HEATING

Smartfit

All components of the Smartfit system are available as spare parts;

T8617B1009 Room Unit 1 day with optimum start
T8677B1006 Room Unit 7 day with optimum start
T8674A1001 Cylinder Sensor
W4672A1009 Base Unit
ML7300A1004 Smartfit Actuator
VU12A1017 2 Way valve, 22mm
VU12A1025 2 Way valve, 28mm
VU13A1015 3 Way valve, 22mm
VU13A1023 3 Way valve, 28mm

Motors

Only one replacement motor (40002737-003) is required for all modern motorised valves irrespective of body size, pipe connection type or whether 2 or 3 ports. An optional 24V AC version is also available (40001011-002).

The 40001011-002 replacement motor is suitable for the old style V8043 and V8044 valves.

Ensure Electrical Safety!

Power Heads

The 40003916 series power heads enable the complete power head assembly to be replaced without draining down on V4043,V4044 and V4073 series valves. On older style valves which did not have a replaceable head feature, the adapter plate assembly can be used to upgrade the valves to allow the replaceable head to be used.

Ensure Electrical Safety!

Thermostatic Radiator Valves

Inserts are available for various types of TRV's. Some of these may be changed without draining the system by the use of a special tool.

WATER PRODUCTS

There are many spare parts available for our range of water products. All available parts are listed in the various catalogues and may be ordered through your normal stockist.

GAS SPARES

IT IS A LEGAL REQUIREMENT THAT GAS APPLIANCE MAINTENANCE AND SERVICING MUST ONLY BE CARRIED OUT BY A CORGI REGISTERED GAS FITTER.

Honeywell is a major supplier of gas valves used in domestic boiler and warm air appliances a position that has been maintained for over 30 years.

Due to the differing requirements for some recent applications, replacement valves may only be available from the original appliance manufacturer. Always check the appliance maintenance instructions before carrying out service work.

Equally important to the correct functioning of gas appliance primary control systems are the pilot burner and thermocouple that operate in conjunction with the gas valve.

Pilot Burners have the type number, e.g. Q359A together with the bracket type and target tip style stamped on them and replacements must always be the same as those fitted as original equipment unless the appliance manufacturer states otherwise. When ordering replacement injectors it is important to identify the pilot burner and whether for LPG or NG.

Honeywell’s Customer Information Centre in the UK has a new central e-mail address, uk.infocentre@honeywell.com which can be used to request details of Honeywell products and services for homes, buildings and industry.

PRIVACY STATEMENT

Copyright © 2005 Honeywell. All rights reserved
smallestlogo.gif (1482 bytes)