Honeywell UK Homepage                             Home Controls Homepage

WHAT WE CAN OFFER


Application Guides

Building Regulations

Combustion Controls

Comfort Controls

End User

FAQ

Industry Links

Installer Training

Instllr./User Guides

Latest News

Literature

Product Families

Spare Parts

Technical Catalogue

Technical Support

Underfloor Heating

Water Products
Product Data

SUNDIAL PLANS DETAIL
 
C Plan

Suitable for new and existing installations with pumped heating and gravity hot water circuits.

C Plan Schematic

c.jpg (9580 bytes)


C Plan Wiring

c1.jpg (20511 bytes)

The Honeywell items used in the installation of this plan will be:

1 - T6360B1028 Room Thermostat
1 - L641A1039 Cylinder Thermostat
1 - V4043H1106 28mm Zone Valve

*Optionallly

1 - 10 Way junction Box - 42002116-001 or
1 - Wiring Centre - 42005748-001
1 - Programmer - ST6400C1003

S Plan

Suitable for fully pumped installations with two primary circuits, usually one for heating and one for domestic hot water.

S Plan Schematic

s.jpg (9394 bytes)

S Plan Wiring

s1.jpg (22912 bytes)

The Honeywell items used in the installation of this plan will be:

1 - T6360B1028 Room Thermostat
1 - L641A1039 Cylinder Thermostat
2 - V4043H1056 22mm Zone Valve

*Optionallly

1 - 10 Way junction Box  -42002116-001 or
1 - Wiring Centre - 42005748-001
1 - Programmer - ST6400C1003

S Plan Plus

Similar to the Sundial S Plan but for use with 3 or more primary circuits, generally two heating zones and one for domestic hot water, Heating zones can be controlled by a combination of time controls and thermostats or by programmable thermostats.

S Plan Plus Schematic

Splus.jpg (10239 bytes)

S Plan Plus Wiring

This is the tham diagram as for the standard S Plan but with additional heating zones as required.

The Honeywell items used in the installation of this plan will be:

2 - T6360B1028 Room Thermostat
1 - L641A1039 Cylinder Thermostat
3 - V4043H1056 22mm Zone Valve

Note: The number of room thermostats and zone valves will be dependent upon the number of heating zones.

*Optionallly

1 - 10 Way junction Box  -42002116-001
1 - Programmer - ST6400C1003

Note: The number of junction boxes and programmers will be dependent upon the number of heating zones.

W Plan

Suitable for fully pumped installations wher it is acceptable to heat only one circuit at a time and normally installed to give priority service to the domestic hot water circuit.

W Plan Schematic

w.jpg (9378 bytes)

W Plan Wiring

w1.jpg (18038 bytes)

The Honeywell items used in the installation of this plan will be:

1 - T6360B1028 Room Thermostat
1 - L641A1039 Cylinder Thermostat
1 - V404C1288 22mm Diverter Valve

*Optionallly

1 - 10 Way junction Box  -42002116-001
1 - Programmer - ST6200A1009

Y Plan

Similar to the W Plan but with the ability to supply both heating and hot water circuits at the same time, if required.

Y plan Schematic

y.jpg (9323 bytes)

Y Plan Wiring

y1.jpg (24203 bytes)

The Honeywell items used in the installation of this plan will be:

1 - T6360B1028 Room Thermostat
1 - L641A1039 Cylinder Thermostat
1 - V4073A1039 22mm Mid position Valve

*Optionallly

1 - 10 Way junction Box - 42002116-001 or
1 - Wiring Centre - 42005748-001
1 - Programmer - ST6400C1003

 

Honeywell’s Customer Information Centre in the UK has a new central e-mail address, uk.infocentre@honeywell.com which can be used to request details of Honeywell products and services for homes, buildings and industry.

PRIVACY STATEMENT

Copyright © 2005 Honeywell. All rights reserved
smallestlogo.gif (1482 bytes)