|
Honeywell can control underfloor heating in many ways. Before
trying to select the controls, it may help to understand the
principle of underfloor heating.
Introduction
to Underfloor Heating
Underfloor
Heating is commonly used in mainland Europe and is becoming
increasingly popular in the UK. It has a number of advantages
and disadvantages over a conventional wet radiator system.
Advantages
-
Even distribution of
heat across the room
-
Easy to install requiring no special skills
-
Unobtrusive
-
No
restriction on the placement of furniture
-
Quiet
in use
-
Very
little maintenance is required
-
Individual room temperature control
-
No risk
of contact with hot surfaces
-
Fabric
temperature of building maintained
Disadvantages
-
Long heat up period
-
Requires major
disruption on existing buildings
-
Long cooling
down period
-
Cannot respond
rapidly to quick temperature changes
-
Choice of
floor finishing requires careful consideration
-
Changes of
floor finish may affect performance.
How does an
Underfloor Heating System Work ?
Generally
speaking, most underfloor heating systems are warm water (wet)
systems although electric (dry) systems are available. For wet
systems, pipes are buried in screed, or run underneath the floor
surface. Underfloor heating systems operate by transferring heat
from a very large surface, which is only slightly hotter than
the room. Radiator systems transfer heat from a very small
surface, which is much hotter than the room, which is very hot.
Typically,
the temperature of the water in the underfloor heating system
pipe is 45 – 65oC (compare this to approximately 80oC
flow and surface temperature of a radiator system) and this
warms the floor to a temperature of 25 – 28oC,
which is comfortable to walk on. In order that the whole floor
area receives heat, the layout of the pipework should be
considered carefully. The supplier of the underfloor pipework
will be able to provide details on the best layout for your
application.
At the design
stage there are a number of points that need to be considered:
-
Insulating affects of floor finish e.g. Carpets
-
Protection of floor finish from cracking
-
Accommodation of thermal gains e.g. conservatory
-
Location
of manifolds
-
Zoning
requirements
-
Boiler/pump position and size
There are
several different pipework layouts which can be used. No matter
what the layout is, this will not affect the control
requirements.
There are
several ways to control an underfloor heating system heating and
these will be discussed later.
Where can
underfloor heating systems be used?
Underfloor
heating systems are suitable for both domestic and commercial
applications. It has a particular advantage in public areas
where exposed hot surfaces can be dangerous.
Gas, oil or
solid fuel boilers can be used as the source of heat for any
underfloor heating system. Condensing boilers being particularly
suited as the operation of underfloor heating systems allows
them to operate in their most efficient manner.
Underfloor
heating systems can be fitted as complete systems in new or
major refurbished properties, extensions to existing houses such
as conservatories or single or multiple rooms in a house.
It is
possible to combine both underfloor systems with radiator
systems. For example, the ground floor could be heated by an
underfloor system whilst the 1st floor is heated
using a wet radiator system or radiators can be fitted in the
bathroom and lavatory in homes where the main system is
underfloor heating.
To control
underfloor heating systems, Honeywell can offer a wide range of
traditional controls and also the more sophisticated Hometronic
system. The selection of these controls for underfloor heating
will be discussed later.
|