Honeywell systems ensure security and spectator
safety in the new Millennium Stadium, Cardiff
(Press Release updated 4th November 1999)
The security of Cardiffs new Millennium Stadium, and
its visitors safety, are assured by advanced systems from Honeywell, the
worlds leading provider of control technologies for buildings, homes, industry,
space and aviation. Honeywell has completed a £2.8 million project, contracted by John
Laing Construction, to supply and install systems for fire detection, security and CCTV
(close circuit television) and PAVA (Public Address Voice Alarm), as well as a system for
the hard of hearing, and distribution of radio, television, data and telephone.
Honeywell began work on the Millennium
Stadium project in 1997 and has been involved at each stage, from evaluating the initial
design brief, through value engineering, design and development of the most cost-effective
solutions, then supplying, installing and commissioning the systems.
Honeywell has now commenced a comprehensive
maintenance contract that includes first-line maintenance of the stadiums
mechanical, electrical, fire and CCTV systems. The scope ranges from fire and security
maintenance to the routine servicing of boiler and air-conditioning. The contract provides
the full-time services of a highly skilled Honeywell engineer, based at the stadium.
Honeywell personnel ensure that the critical life safety equipment is maintained during
Stadium events, which can range from rugby to pop concerts.
The Honeywell fire system at the stadium is
fully addressable, linking 2383 devices into seven networked fire control panels. It
includes an integrated fire telephone communication system in each of the stadiums
fire fighting stairs and on every level. An alarm initiated from any detector is displayed
on all seven fire alarm panels. The user interface is a LAN (local area network) based PC
system, which shows graphically the exact location of a device in alarm. The system
provides L1 cover to BS5839 and EN54 regulations.
The fire system can operate manually or
fully automatically to initiate evacuation of the public. The systems
"voice" is a PAVA system providing emergency announcements (including
instructions for evacuation) and other pre-recorded messages.
The security system is based on a Honeywell
Excel Security Manager (XSM) with 70 zones. This PC-based system protects the stadium from
unauthorised entry on levels 1, 2 and 3. It uses numerous door contacts and passive
infra-red detectors (PIRs) to detect intruders. The XSM interfaces with the CCTV system so
that a camera is repositioned automatically to show the area of a security breach.
The CCTV system was developed by Honeywell
in consultation with the Stadium safety committee, the local police authority and the
Guide to Safety at Sports Grounds ("The Green Guide"). It has 60 cameras, of
which six cover the arena (bowl) area, and can be operated, from control rooms on levels
one or five.
The Hard of Hearing system is the first of
its kind in the UK to operate on dedicated radio frequencies allocated by the RCA and has
EMC certification. The system provides an audio feed appropriate to the event (such as a
radio commentary) and is interrupted automatically to carry essential emergency messages
from the public address system. Initially, the system has provision for 200 receiver
units, which are loaned to the public as required. Elements of this versatile,
programmable system ensures that there are no seating restrictions in the arena for the
hearing impaired spectators.
The PAVA system has 1600 speakers covering
the entire stadium complex and complies fully with BS5839, BS7443 and BS7827. It is
distributed and operated digitally from either control room. The system features a touch
screen facility so that areas of the stadium can be paged with safety and other
information, as appropriate.
The radio/TV distribution system comprises
210 outlets. The press areas, home and away changing rooms, banqueting suites and all the
Stadiums 125 private boxes have radio/TV outlets capable of providing terrestrial
and satellite broadcasts. The rear of the lowest terrace is fitted with TV outlets to
enhance spectators enjoyment.
To interconnect all the points associated
with the various systems, Honeywell has installed a structured cabling system for voice
and data, with a fibre-optic backbone interconnecting 15 communications rooms within the
Stadium complex. These rooms house Honeywells apparatus and cable distribution
frames that provide complete flexibility of configuration.
Honeywell Control Systems Ltd., founded in 1936, is the UK operation of
Honeywell Inc., the worlds leading provider of control technologies for buildings,
homes, industry, space, and aviation. The company employs 57,000 people in 95 countries,
and had 1998 sales of $8.4 billion. Honeywell employs over 2,900 people in the UK and the
Republic of Ireland, and has a manufacturing and development centre at Newhouse in
Lanarkshire.
For further information please contact:
Royer Slater (direct phone: 01344 656379;
direct fax: 01344 656034)
Honeywell Control Systems Ltd
Honeywell House
Arlington Business Park
Bracknell
Berkshire RG12 1EB
Switchboard: 01344 656000. Fax: 01344 656240.
E-mail: Personal: royer.slater@uk.honeywell.com
General: uk.infocentre@honeywell.com
Web: www.honeywell.com |